Tool/software: TI C/C++ Compiler
Hi Alex:
I have several problems now and I need your help!
1. A brief description of the light source: we use the light source USES a laser to transmit and receive Angle are 5 °, when working under the condition of the maximum current (173.6 mA), the optical power of about 100 mw, the measurement is 10 ~ 15 meters AMP_OUT is about 300, PHASE_OUT is about 44000, is this because of our impact on the circuit design?The front-end AFE is designed to work at 100mW what should the theoretical AMP_OUT value be close to?
2. Regarding the problem of mass production, since all four currents need to be calibrated in super-hdr mode, can the four currents be calibrated at a fixed distance?If possible, I would like to know the value of IPHASE and QPHASE after xtalk calibration.If not, can you give us a better mass production plan?
Thanks,
Best,
Kevin