I've already tested the PGA460 with your EVM.
I'm now trying to develop my own PCB and my own firmware.
Following your SLAA730A software development guide, I'm getting the ultrasonic measurament with the following
1) PGA460_sensorParameters()
2) PGA460_Init_Thresholds()
3)PGA460_initTVG()
3) Master transmit a Preset 1 burst and listen command for 1 object (CMD 1): 0x{55 00 01 FE}
4) Delay(100)
5) Master requests slave to return the ultrasonic measurement results (CMD5): 0x{55 05}
I assume that this is based in the initial gain, isn't it?
The next step is to procceed with TVG procedure. Which is the procedure?