This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: SDK Ver 1.1.0.2 Vs 2.0

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642

Hi,

We are currently working with an application which was developed under SDK 1.1.0.2.

Is it possible to run  this application with a new IWR1642 board, which is SDK 2.0 based?

We got The indication that it is SDK 2.0 from trying to see point cloud (demo) with

Demo visualizer of version 1.1, and got the error message of SDK version mismatch.

In other words, is there a possibility that an IWR boost board (SDK Ver 2.0 based), will not support

Some older SDK versions (1.0.0.2)?

Thanks,

Boaz