Other Parts Discussed in Thread: , MMWAVE-SDK, UNIFLASH, IWR1642, IWR1642BOOST, TIDEP-0090
Help Needed I am a Hardware Development Engineer, working alone. Trying to Prove a Concept.
I'm not very good at software/firmware development.
I have an AWR1642BOOST EVM. It is a few months old and probably ES1.0, Can't read the writing on the AWR1642 chip, it is not visible.
Also have a mmwave-devpack, the box shows seal date 6/17/17 – I would have to “destroy” the AWR1642 by removing 3 resistors in order to adopt the EVM for use with the devpack, so I prefer not to use the devpack if not essential.
Need to extract Three approaching “Targets”, which may be Automobiles or People: the closest, the fastest and the largest. The resulting range, (radial) velocity, and size of each of these three targets then need to be recognized as data that can be read by further, “back end” processing continuously.
Need to update the processing for every frame.
Long Range and High Velocity is sought, Resolution is secondary. No specific distance or speed, just for now, the longer range and higher velocity it can handle is a plus.
Can this EVM be configured to do this?
Is “gtrack.h” sufficient to Generate and Track the three Targets?
Is the AWR1642 ES2.0 required?
Will this Hardware or Software be revised soon to an ES3.0?
Is the DCA1000 EVM Real-Time Data-Capture Adapter for Radar Sensing Evaluation Module Required? (Hope not)
It is not essential to do this proof of concept with an AWR1642, It will not be on an Automobile. Maybe IWR or other EVMs can achieve this result.
TI has downloaded
Per tools/mmwave-sdk, “MMWAVE-SDK-LTS” 1.02.00.05, 07 MAR-2018
Long Term Support, which Supports AWR1642 ES1.0
Also “MMWAVE-SDK” 2.00.00.04, 26 APR-2018 (If I need the ES2.0, Rev A AWR1642)
Demo Visualizer
CCS 8
Uniflash
I have a Windows 7 laptop, i7. Using Chrome.
Need to first run this as a Demo on the Laptop.
Once this demo is seen to be Extracting Targets on the Demo Visualizer Console, the demo will need to be converted to run in Linux in order to combine the target data output with the “back end” processing. At that point, the Demo Visualizer may not be required.
Will someone please assist me in accomplishing this task?
Thank You,
Dan