Other Parts Discussed in Thread: AWR1642
When setting chirp profile configuration, I get the error ''SAMPLING RATE IS NOT WITHIN [2, 37.5] Msps'' when I have entered a sampling rate of 10000ksps, which is evidently within the range [2,37.5] Msps. The error is resolved when i change the sampling rate to 5000ksps, but I don't see why there should be an upper bound for the sampling frequency.
[17:44:42] [RadarAPI]: Opening Gpio Control Port()
[17:44:42] [RadarAPI]: Status: Passed
[17:44:43] [RadarAPI]: Opening Board Control Port()
[17:44:43] [RadarAPI]: Status: Passed
[17:44:44] [RadarAPI]: ar1.FullReset()
[17:44:44] [RadarAPI]: Status: Passed
[17:44:44] [RadarAPI]: Closing Board Control Port()
[17:44:44] [RadarAPI]: Status: Passed
[17:44:45] [RadarAPI]: Closing Gpio Control Port()
[17:44:45] [RadarAPI]: Status: Passed
[17:44:45] [RadarAPI]: ar1.SOPControl(2)
[17:44:45] [RadarAPI]: Status: Passed
[17:44:45] [RadarAPI]: ar1.Connect(4,921600,1000)
[17:44:48] [RadarAPI]: Warning: Connected with baudrate 115200
[17:44:49] [RadarAPI]: Warning: Disconnected existing BaudRate
[17:44:49] [RadarAPI]: Warning: Trying to connect with baudrate 921600
[17:44:50] [RadarAPI]: ar1.Calling_IsConnected()
[17:44:51] [RadarAPI]: ar1.SelectChipVersion("XWR1642")
[17:44:51] [RadarAPI]: Status: Passed
[17:44:52] [RadarAPI]: ar1.SelectChipVersion("XWR1642")
[17:44:52] [RadarAPI]: Status: Passed
[17:44:52] [RadarAPI]: ar1.SaveSettings('C:\Users\WORK\AppData\Roaming\RSTD\ar1gui.ini')
[17:44:53] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\radarss\\xwr16xx_radarss_rprc_ES1.0.bin")
[17:44:53] [RadarAPI]: Downloading BSS ROM RPRC Binary..
[17:45:00] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\masterss\\xwr16xx_masterss_rprc_ES1.0.bin")
[17:45:00] [RadarAPI]: Downloading MSS RPRC Binary..
[17:45:05] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[17:45:05] [RadarAPI]: Status: Passed
[17:45:05] MSS power up done async event received!
[17:45:05] [RadarAPI]: ar1.SaveSettings('C:\Users\WORK\AppData\Roaming\RSTD\ar1gui.ini')
[17:45:06] [RadarAPI]: ar1.RfEnable()
[17:45:06] BSS power up done async event received!
[17:45:06] [RadarAPI]: Status: Passed
[17:45:15] [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 1, 0)
[17:45:15] [RadarAPI]: Status: Passed
[17:45:16] [RadarAPI]: ar1.LPModConfig(0, 0)
[17:45:16] [RadarAPI]: Status: Passed
[17:45:17] [RadarAPI]: ar1.RfInit()
[17:45:17] RF Init async event received!
[17:45:17] [RadarAPI]: Status: Passed
[17:45:17] [RadarAPI]: Time stamp, Temperture: 10857,29; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; RxIQMM Status, Update: 1, 1;
[17:45:20] [RadarAPI]: ar1.DataPathConfig(513, 1216644097, 0)
[17:45:20] [RadarAPI]: Status: Passed
[17:45:21] [RadarAPI]: ar1.LvdsClkConfig(1, 1)
[17:45:21] [RadarAPI]: Status: Passed
[17:45:22] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 0, 0, 1, 0, 0)
[17:45:22] [RadarAPI]: Status: Passed
[17:45:27] [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30)
[17:45:27] Status: Failed, Error Type: SAMPLING RATE IS NOT WITHIN [2, 37.5] Msps
[17:51:59] [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 5000, 0, 0, 30)
[17:51:59] [RadarAPI]: Status: Passed