Part Number: OPT8241-CDK-EVM
Greetings,
I need help to determined the best parameters according to my scenario:
The goal is to determined the height of an object in movement (that's why I can't go down 30fps ) in a relative small area.
The height of the object will be from 90cms to 170cms however it can be up to 4m far from the sensor!
In the worst case, the sensor will be used outside at 90° compared to the sun.
I'm looking for a precision of 5 cms maximum, what precision can I expect according to these specifications ?
I saw that the CDK isn't calibrated for best accuracy, should I consider to do it even if I'm using one of the default profile (I guess the best one for my application is long range )
Thanks in advance.