Dear All,
May I know if any of our Inductive Sensing IC can be utilized for detective a small Screw made of Titanium Metal?
The Screw Length would be in the range of 5 to 10 mm, and the Screw Diameter is approximately 2 to 3 mm.
I need the absence / presence detection, but if it can detect sensor to target distance which will be always less that 10 mm, it would be great!!!
I do not think there is any necessity of using a Micro-Controller. An Inductive Metal Detector IC, working from a single 3 V Lithium-Ion Coin Battery would be OK for a small hand-held pen-like device.
Kindly advise as below:
1] Can the Metal Part as small as a Screw, of Titanium Metal, be detectable with any of the circuits based on any of our ICs?
2] If yes, which IC Part Number would be the Best or a Good Choice to try-out by me?
3] Any other tips and / or tricks which you can please share with me on this subject?
Sincerely awaiting your important and valuable technical feedbacks.
Thanks & with best regards, - Jay.