This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443: Configuration file not working

Part Number: AWR1443

Hi,

I used the mmwave demo visualiser to generate a config file and load it onto my AWR1443. However, the file crashes immediately after sensorstart. I do not know the reason for this behaviour. The config file is attached below for your reference.

% ***************************************************************
% Created for SDK ver:01.01
% Created using Visualizer ver:2.0.0.2
% Frequency:77
% Platform:xWR14xx
% Scene Classifier:best_range
% Azimuth Resolution(deg):15
% Range Resolution(m):0.244
% Maximum unambiguous Range(m):50
% Maximum Radial Velocity(m/s):1
% Radial velocity resolution(m/s):0.13
% Frame Duration(msec):100
% Range Detection Threshold (dB):15
% Range Peak Grouping:enabled
% Doppler Peak Grouping:enabled
% Static clutter removal:disabled
% ***************************************************************
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 5 0
adcCfg 2 1
adcbufCfg 0 1 0 1
profileCfg 0 77 465 7 21.85 0 0 44.4 1 256 18500 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 4
frameCfg 0 1 16 0 100 1 0
lowPower 0 0
guiMonitor 1 1 0 0 0 1
cfarCfg 0 2 8 4 3 0 1280
peakGrouping 1 1 1 1 229
multiObjBeamForming 1 0.5
clutterRemoval 0
calibDcRangeSig 0 -5 8 256
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
sensorStart

The error that I get is as follows:

Could someone pllease help me work around this ?

Thanks