Hi
Our custoemr has following questions about TMP431.
1.
Figure 7 and 9 in datasheet offer remote temperature error against Rs and Cdiff.
Regarding to the remote temperature error in figure 7,does it mean that reading value from the remote temperature register is larger 2 degree than the actual temperature on remote IC?
2.
How to consider maximum remote temperature error?
According to datasheet, TEremote is offered by +-5 degree as maximum.
Is it possible to consider TEremote is upper limit of the remote temperature error?
Or, should we consider additional factor for the remote temperature error?
3.
The customer faced the circumstance that the remote temperature error is increased
as higher ambient temperature (over 80 degree).
what is caused mainly?
BestRegards