I am trying to capture the Raw ADC data in real time. What I want to do is configure the waveform parameters and read the ADC parameters via MATLAB. I want to do the real-time processing by frame to frame basis. Basically, what I want to do is verify if one of the high-resolution AOA estimation algorithms I wrote works with the device or not. For this, I need real-time data capture and its post-processing.
Can you please guide me how could I perform this. Using Radar studio, I am not able to get the data in real time. As in, I get all the data at once. But I want real-time processing. What can I do about this? Would capture data using CCS help? If yes, what approach should I be using here?
Secondly, if I use CCS, would I be needing only AWR1642Boost board?
Thirdly, I don't have the DCA1000 board for real-time capture, and due to the limited timeline of the project, I won't be able to procure it in time. All I have is AWR1642Boost, mmWave-DevPack and TCW1400EVM.
Any help would be appreciated
Thanks