This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1642BOOST: Vital Sign CCS PROJECT BUILD ERROR

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: MMWAVE-SDK, AWR1642, IWR1642

Tool/software: Code Composer Studio

Hi,

I have imported Vital Sign project from TI Resource Explorer and trying to build it but it is giving following error. 

>> Compilation failure
subdir_rules.mk:30: recipe for target 'main.oer4f' failed
"../main.c", line 1135: warning #188-D: pointless comparison of unsigned integer with zero
"../main.c", line 1676: error #20: identifier "rlRfInitomplete_t" is undefined
"../main.c", line 1676: error #20: identifier "ptrRFInitCompleteMessage" is undefined
"../main.c", line 1680: error #29: expected an expression
"../main.c", line 1680: error #66: expected a ";"
4 errors detected in the compilation of "../main.c".
gmake[1]: *** [main.oer4f] Error 1
'Building file: "../config_hwa_util.c"'

Here are compiler settings and SDK version

'Invoking: ARM Compiler'
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=32 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/LaxmiKant/Google Drive/CCSv7/vitalSigns_lab" 
--include_path="C:/ti/mmwave_sdk_02_00_00_04/packages" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR14XX --define=SUBSYS_MSS
--define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_SIZE=0x40000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN -g --diag_warning=225
--diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=packed --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="config_hwa_util.d_raw"
--cmd_file="configPkg/compiler.opt" "../config_hwa_util.c" 'Finished building: "../config_hwa_util.c"'