Customer using the latest version of mmWave toolbox, lab11. They have a new IWR1642BOOST that I believe is ES2.0.
When testing using 6m_ConferenceRoom.cfg everything works as expected, and the max detection distance is about 6m. But when we try to extend the range, using 14m_Hallway.cfg or 14m_OfficeSpace.cfg - they can’t establish stable detection on 6m and further. They have found hard coded 6m max sensor range value in demo source code, but even changing it to relevant value doesn’t help.
Today, running the demo with 14_OfficeSpace.cfg they could not detect moving human 3m just in front of the board.