Hi. everyone.
I'm using the OPT3101EVM.
There is an equation about distance in the datasheet.
What is the "c", speed of light value in the datasheet? The distance equation is (PHASE_OUT/2^16)/(c/10Mhz) meters.
Our solution is that measure the distance of hot Slab which is a high temperature. (Max 400℃)
Is it possible to measure the hot slab?
Best
Regrads