This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: Failed to load images using UniFlash.

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: UNIFLASH

Hi,

  For some reason, after I switched off the device, I am unable to reload images.

  I am keep getting error messages such as "Image loading failed: Not able to connect to serial port.  Recheck COM port selected and/or permissions".

  Here are things I have tried.

  1. Check DeviceManager and load COM port appropriately.

  2. Uninstall XDS UART and XDS Data port and reinstall

  3. Rebooting the computer.

  Reading another forum answer seemed to resolve this issue when CSS is not being turned on when running UniFlash.  However, I'm still seeing the same error message.

  Any idea?

  Thanks,

DJ