Other Parts Discussed in Thread: AWR1642, SYSBIOS
Tool/software: Code Composer Studio
I received the error "Mailbox_handle" is undefined when trying to build the DSS project for the Vital Signs demo. Initially, I flashed the pre-built binaries on to my AWR1642 and was able to successfully demonstrate the lab. The next thing I wanted to do was download the project, build it, and flash my built image onto the AWR1642 to verify that both methods work. While compiling the DSS, I ran into this error and I am unsure how to troubleshoot. I have downloaded mmWave SDK 2.0.0.4, AWR1642 ES1.0, and CCS v8, so I think I should have all of the software and hardware requirements necessary to complete the build. The only thing that I could think is wrong is that the newest version of SDK (2.0.0.4) is not compatible with the older version that the demo calls for (1.1.0.2). Has anyone run into this problem that has managed to solve it? I would greatly appreciate any help.