Part Number: OPT8241-CDK-EVM
Hi everyone,
I don't understand the negative 5V bias. Is it used like a contrast voltage in an LCD? Why is it also used on the connector to the illumination board?
Thx in advance,
Bernd
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thank you for your quick reply!
Is it recommended to be able to set the voltage between 0 and -5V? I'd otherwise like to use the LM27761 chargepump and bias the feedback resistors using a spare LDO. This way I could save the digital pot (TPL0102-100PWR) and its corresponding levelshifter. I'd be able to set the voltage from -5.062 V up to -2.87 V. The LM27761 can deliver up to 250mA.
Do you think these parameters are sufficient? What voltage is used in the CDK? I wasn't able to find the potentiometer register beeing set (I had a look here).
Regards,
Bernd