This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: Effects of Antenna Etch tolerance

Part Number: IWR1443
Other Parts Discussed in Thread: , IWR1642

The Antenna_Etching_Requirements.docx document in the fab folder indicates that a +-20um tolerance is required for the antenna. Is there any data available about what would happen to the antenna performance if this tolerance was to be relaxed? 

For our application we only need a couple meters of range with +- 5cm of accuracy for obstacle detection so I would think we could relax this tolerance some but I would like to have some data on how much it can be relaxed.

We are very concerned with cost on this device and this tolerance on the antenna seems to be a pretty big driver on the board price.

Thanks

  • Hello Kevin,

    The RF structure Grounded Coplanar Waveguide, stripline extension to antenna, and the antenna all contribute to the Tx and Rx return loss.  The return loss has both an RF band 77-81Ghz, where there is more than (6) 10db S11.  

    We have seen that over and under etching of the antenna can result in a phase difference, and higher losses.  

    When you make the PCB, there is an RF stripline structure, for checking the PCB fabrication, so the return loss of this stripline can be measured.

    There is a SPRACG5 mmwave Radar sensor RF PCB Design, Manufacturing and Validation Guide.    The guide indicates that tight tolerances are recommended, for a new EVM, we have the PCB fabricator check the bare board, against a dimensioned drawing.   We normally use a 1mil tolerance for this test.  

    The Rogers 4835 LoPro, 4mil dielectric, 1/2oz Copper  - to use the  EVM RF traces/antenna, you need to use this RF Laminate material.

    If your design has a max range of < 10meters, Field of view for azimuth and Elevation of ~120 degrees, and you want a simpler to fabricate antenna.   You can use a single patch design for the (4) Rx, and (2 or 3) Tx.    Please look at the EVM User Guide swru518c Figures 11, 12 for the existing EVM.  

    The vertical patches combine in phase to reduce the elevation field of view.   If you make each one a single patch, there is less geometry for the under and over etching to affect.    There are 6 sets of Rx; outside left shield, Rx1, Rx2, Rx3, Rx4, outside right shield.  The Tx orientation allows for Tx1, Tx3 for MIMO.  Tx2 is for elevation.  All of these could be a single patch, reducing the board size and complexity.

    The spracg5 document discusses EM simulation.   There are several papers that discuss antenna geometry, field of view, some discuss that a 15um disturbance can be measured in the testing of the patch antenna.  

    suggestion: if you want to first copy the EVM antenna, and RF traces, use the 1mil error criteria

                        if you want to build an EM simulation from the DXF single antenna attached, you could introduce for a single patch other errors.

    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/1023/iwr1443boost_5F00_reva_5F00_dxf.dxf

    I have attached a System Estimator example for 15meters, RCS .1, IWr1443, 4Rx, 2Tx , Range Resolution 4.5cm, with the 5dbi Tx and Rx gain.

    At the top right the Max range is calculated at 26meters, with an RCS target minimum of .11.

    Sensing Estimator Tool "  dev.ti.com/.../   " 

    Attached configuration is loaded for System design - "iwr1443_15m_4Rx_2Tx_4p5cm.json"

    {
        "platform": "xWR1443",
        "num_rx": 4,
        "num_tx": 2,
        "tx_gain": 5,
        "rx_gain": 5,
        "frequency_range": "77 - 81",
        "maximum_bandwidth": 4000,
        "tx_power": 12,
        "ambient_temperature_degC": 70,
        "maximum_detectable_range": 15,
        "range_resolution": 4.1,
        "maximum_velocity_kmph": 10,
        "velocity_resolution_kmph": 2,
        "measurement_rate": 10,
        "typical_detected_object": ".1",
        "detection_loss": 2,
        "system_loss": 2,
        "implementation_margin": 2,
        "detection_SNR": 14,
        "maximum_radar_cube_size": 256,
        "maximum_RF_bandwidth": 15,
        "maximum_sampling_frequency": 18.75,
        "sensor_maximum_bandwidth": 4000,
        "maximum_allowed_bandwidth": 4000,
        "starting_frequency": 77,
        "maximum_velocity": 2.7777777777777777,
        "velocity_resolution": 0.5555555555555556,
        "idle_time": 7,
        "adc_valid_start_time": 12.2,
        "excess_ramping_time": 1,
        "periodicity": 100,
        "ambient_temperature": 343.15,
        "noise_figure": 16,
        "num_virtual_rx": 8,
        "non_coherent_combining_loss": 3,
        "rcs_value": 1,
        "combined_factor_in_dB": -17,
        "combined_factor_linear": 0.0199526231496888,
        "valid_sweep_bandwidth": 3658.5365853658545,
        "inter_chirp_time": 20.2,
        "aux_comp_coeff_a": 78829268292.68292,
        "aux_comp_coeff_b": -11863014.634146342,
        "chirp_time": 150.48997524752477,
        "ramp_slope_init": 24.310832527869856,
        "ramp_slope_parameter": 504,
        "ramp_slope": 24.33300018310547,
        "aux_comp_T1": 1,
        "maximum_beat_frequency": 2.433300018310547,
        "sampling_frequency": 2.7036666870117188,
        "number_of_samples_per_chirp": 407,
        "total_sweep_bandwidth": 3984.195602416992,
        "idle_time_minimum": 7,
        "ramp_end_time": 163.73630758377425,
        "carrier_frequency": 77.2968638450859,
        "aux_comp_T2": 6.2,
        "adc_valid_start_time_2": 7.2,
        "lambda": 3.881140644997492,
        "max_chirp_repetition_period": 349.3,
        "chirp_repetition_period": 341.5,
        "num_range_fft_bins": 512,
        "min_num_of_chirp_loops": 11,
        "max_range_for_typical_detectable_object": 26.188911143061215,
        "min_rcs_detectable_at_max_range": 0.10762056499385238,
        "num_doppler_fft_bins": 16,
        "active_frame_time": 5.464,
        "range_inter_bin_resolution": 3.2591796874999996,
        "velocity_inter_bin_resolution": 0.3819444444444445,
        "radar_cube_size": 176
    }

  • Thanks for the feedback, I have a few additional questions below.

    Radio-Joe said:

    We have seen that over and under etching of the antenna can result in a phase difference, and higher losses.  

    Do you have any data about how much losses  could be expected for different over and under etching amounts?

    Radio-Joe said:

    If your design has a max range of < 10meters, Field of view for azimuth and Elevation of ~120 degrees, and you want a simpler to fabricate antenna.   You can use a single patch design for the (4) Rx, and (2 or 3) Tx.    Please look at the EVM User Guide swru518c Figures 11, 12 for the existing EVM.  

    The vertical patches combine in phase to reduce the elevation field of view.   If you make each one a single patch, there is less geometry for the under and over etching to affect.    There are 6 sets of Rx; outside left shield, Rx1, Rx2, Rx3, Rx4, outside right shield.  The Tx orientation allows for Tx1, Tx3 for MIMO.  Tx2 is for elevation.  All of these could be a single patch, reducing the board size and complexity.

    Is there a reference design available for the single patch configuration? Our application could benefit from a greater vertical field of view.

    Radio-Joe said:

    The spracg5 document discusses EM simulation.   There are several papers that discuss antenna geometry, field of view, some discuss that a 15um disturbance can be measured in the testing of the patch antenna. 

    It makes sense that a small disturbance in the geometry would be easily measurable, the question for us is will that performance degradation be acceptable for our application so I could use some numbers here describing how much it will be affected.

    Additionally, the DXF that you posted seems to be empty. Could you please re-post the file.

    Thanks,

    Kevin

  • Hello Kevin,
    I will have to ask others about the > 1 mil tolerance effects, I think we have some 1642 antenna results. It will take a few days to find.

    The single patch antenna I will ask the antenna designer, normally the 1443, 1642 have more vertical patches to limit the elevation field of view.

    I would not try the multiple patch Rx or Tx, with > 1mil, It caused side lobes, I will try to get a report to send. Single patch may be better.

    I have also asked for a regenerated DXF file.

    I will send more before the end of the week.
    Joe
  • Hello,

    Here is the single element patch.  You can put this into an HFSS simulation to look at the Field of View, estimated S11 return loss, and estimated antenna gain.   Note: in replacing the IWR1443 antenna, please remember to match the Tx to Tx trace lengths within 1 mil, and separately to match the Rx to Rx trace lengths to 1mil.

    Still looking for the other report.

    Regards,

    Joe Quintal

    RO4835_1E.zip

  • Thanks for the drawing. Unfortunately we are a small company and I do not have access to HFSS or other RF simulation software to simulate the antenna.
  • Hello,
    In previous EVM work, we found that a 2 mil deviation from dimensions or delamination of the antenna patch would make the IWR1642 antenna not functional.

    Note: this was for a multi-patch / per Tx or Rx antenna. There were changes in the antenna sensitivity that required the antenna to be repointed, and the object detection had impairments, more reflected objects.
    Regards,
    Joe Quintal