Tool/software: Linux
hi ,
when I compiler the 3dtof/voxelsdk sdk ,I got the problem below,I use the ubuntu 14 , and I have tried some ways to fix this problem but that seems not work ,can anyone give some advices ,I have a
opt8241 evaluation board ,and I want to get the data with my arm board ,can you give me simple samples to got the data frome opt8241, thank you !
Scanning dependencies of target ti3dtof
[ 62%] Building CXX object TI3DToF/CMakeFiles/ti3dtof.dir/VoxelProgrammerBase.cpp.o
/home/jason/TI-tof/libvoxel/voxelsdk/Voxel/SWIG/../Device.h:63: Error: Syntax error in input(3).
make[2]: *** [lib/python2.7/VoxelPYTHON_wrap.cxx] Error 1
make[1]: *** [Voxel/SWIG/CMakeFiles/_Voxel.dir/all] Error 2
make[1]: *** Waiting for unfinished jobs....
[ 63%] Building CXX object TI3DToF/CMakeFiles/ti3dtof