This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AWR1642BOOST: Saving raw ADC data from CCS Memory using MATLAB

Part Number: AWR1642BOOST

Tool/software: Code Composer Studio

I have been able to setup the serial port, send the configuration parameters to CCS for reading the ADC data. 

The memory location is updated. However, I still have to save the data manually in CCS. Is it possible to save this raw ADC data as well using MATLAB?

 

Many Thanks

  • Anum,

    The capture demo is not being actively supported since it is not a current release of our SDK or an SDK under LTS (long-term support). The existing whitepaper that I have pointed out before describes the process for observing the ADC data being stored in L3 memory. It also provides MATLAB example code on how to read ADC data that is output by the TSW1400. TI does not provide MATLAB code for exporting data from CCS memory since this task can be completed natively in CCS.

    Regards,
    Kyle