Hi!
I have few questions.
I use GUI version 1.2.7.1.
To sense the fluid level, i downloaded Matt Minasi's config. (TDC1000-7200_level_cells_saleskit_2_2015.txt)
When i go to the TANK LEVEL tab after starting graph, the current level is fixed at 2.18cm.
I try to add or reduce water in plastic tank i used, but it still fixed at 2.18cm. And there is TANK EMPTY message on GUI.
I think the sensor is mounted at tank well. But it didn't work. TANK EMPTY means what?
Also in graph tab, Is the unit of TOF AVG VALUE nano second?
When i change water level, TOF VALUE's change amount is very small. So i can't calculate the exact water level using that value.
If it is related to the strange TANK LEVEL, how can i fix it?
One more question, what FLOW MODE means?
Using that mode, graph's Y axis is changed and DELTA TOF VALUE is shown.
What is the difference from original mode?
Best regards,
Shin A