Hey,
I am trying to find a suitable solution for heating and cooling of a special part of my circuit. For that, I have chosen a Peltier element and would like to use an H-Bridge IC with a PWM Control. Do you have a suitable IC for the regulation of the Peltier element?
I’ve attached the datasheet of this Peltier element.
Additional features that the circuit should have:
- H-Bridge: I should be able to have only 3 states: Heat-Up, Cool-Down or do nothing. I.e. the short-circuit should be disabled.
- H-Bridge should be controlled via PWM.
Any help, like reference design, is much appreciated since I’ve never worked with Peltier elements and now we need to integrate them into more than 10 000 devices with really little time for prototyping.
Kind Regards,
Den