This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP300: TMP300 output

Part Number: TMP300


Hi,When TMP300 reaches the set temperature, is OUT low or high,could you help check it,tks!

  • Hi,

    The output of the TMP300 is normally high and is pulled low when the temperature threshold is tripped. You can see this by observing the open-drain output, which uses a pull-up resistor, which pulls the OUT pin high when the chip is floating (when the switch is not tripped).

    Thanks for the question!

    Audrey