Other Parts Discussed in Thread: AWR1243BOOST, , AWR1243, UNIFLASH
Hello,
Today I managed to partially get my AWR1243BOOST and DCA1000 set up working but I hit some errors around the successful uses as well.
1. Immediately upon powering up the boards the red NERR LED on the AWR1243BOOST board is lit. When I attempt to connect the SPI I obtain a time out error (see the first attached log). When reset in the GUI is pressed once again though the red NERR LED goes out and SPI connection can occur. Pressing reset in mmWave studio before attempting the SPI connection the first time doesn't change anything (i.e. SPI connection must fail, then reset is pressed, then SPI can connect).
2. I keep getting an error message that the ethernet cable is disconnected (when using the setup DCA1000 window) even though the cable is in securely. Restarting mmWavestudio occasionally fixed this, after many failures at the same point and restarting mmWave studio a few times I got the ethernet connection to be recognised and had three successful runs using the data capture demo script. However it then seemed that the the etherrnet connection was dropped and a subsequent attempt ended in failure (See second attached log).
3. After some more opening and closing mmWave studio and power cycling the boards (Having to deal with error number 1 each time power was cycled) the ethernet connection was again usable and many runs were succesful (see third attached log).
4 Now, the ethernet connection appears to be connected (i.e. there is no error message saying it's disconnected and the DCA1000 setup screen is as described in the user guide) but when a frame is triggered the LVDS Buffer overflow LED lights red and in the output window I get the message: STS_LVDS_BUFFER_FULL Async event recieved(9) (see the fourth attached log
GM: Constructor
GM: Thu Aug 09 13:13:58 2018
RSTD.Transmit("/Settings")
[13:13:59]
[13:13:59] ### Running Startup script: "C:\ti\mmwave_studio_01_00_00_00\mmWaveStudio\Scripts\Startup.lua" ###
[13:13:59] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[13:13:59] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[13:13:59] Scripter ignored: Attempt to UnBuild() again or before Build.
[13:13:59] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
[13:13:59] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[13:13:59] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[13:13:59] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[13:13:59] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[13:13:59] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[13:13:59] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\RunTime\\SAL.dll")
[13:13:59] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[13:13:59] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[13:13:59] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[13:13:59] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[13:13:59] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[13:13:59] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[13:13:59] RSTD.Transmit("/")
[13:13:59] RSTD.SaveSettings(): Settings saved to "C:\Users\Matthew\AppData\Roaming\RSTD\config.xml"
[13:13:59] RSTD.Build()
[13:13:59] RSTD.SaveSettings(): Settings saved to "C:\Users\Matthew\AppData\Roaming\RSTD\config.xml"
[13:13:59] RSTD.Transmit("/")
[13:13:59] RSTD.AL_Build()
[13:13:59] RSTD.AL_LoadXml()
[13:13:59] RSTD.Transmit("/")
[13:13:59] RSTD.AL_Init()
[13:13:59] RSTD.Clients_Build()
[13:13:59] GM: Init
[13:13:59] GM: Loaded 'C:\ti\mmwave_studio_01_00_00_00\mmWaveStudio\Clients\\LabClient.dll'
[13:13:59] GM: 1 Guest (s) init
[13:13:59] GM: 1 Module(s) init
[13:13:59] GM: 2 Tab (s) init
[13:13:59] RSTD.Client_LoadXml()
[13:13:59] [RadarAPI]: Starting Matlab Engine..
[13:15:31] [RadarAPI]: Matlab Engine Started!
[13:15:40] [RadarAPI]: ar1.LoadSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[13:15:41] TESTING = false
[13:15:41]
[13:15:41] ***Script completed successfully.***
[13:15:52] [RadarAPI]: Opening Gpio Control Port()
[13:15:52] [RadarAPI]: Status: Passed
[13:15:52] [RadarAPI]: Opening Board Control Port()
[13:15:52] [RadarAPI]: Status: Passed
[13:15:53] [RadarAPI]: ar1.FullReset()
[13:15:53] [RadarAPI]: Status: Passed
[13:15:54] [RadarAPI]: Closing Board Control Port()
[13:15:54] [RadarAPI]: Status: Passed
[13:15:54] [RadarAPI]: Closing Gpio Control Port()
[13:15:54] [RadarAPI]: Status: Passed
[13:15:54] [RadarAPI]: ar1.SOPControl(2)
[13:15:54] [RadarAPI]: Status: Passed
[13:15:57] [RadarAPI]: ar1.Connect(4,921600,1000)
[13:16:00] [RadarAPI]: Warning: Connected with baudrate 115200
[13:16:01] [RadarAPI]: Warning: Disconnected existing BaudRate
[13:16:01] [RadarAPI]: Warning: Trying to connect with baudrate 921600
[13:16:02] [RadarAPI]: ar1.Calling_IsConnected()
[13:16:04] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[13:16:04] [RadarAPI]: Status: Passed
[13:16:04] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[13:16:04] [RadarAPI]: Status: Passed
[13:16:05] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[13:16:07] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\radarss\\xwr12xx_xwr14xx_radarss_ES2.0.bin")
[13:16:08] [RadarAPI]: Downloading BSS ROM Legacy Binary..
[13:16:15] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\masterss\\xwr12xx_xwr14xx_masterss_ES2.0.bin")
[13:16:16] [RadarAPI]: Downloading MSS Legacy Binary..
[13:16:45] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[13:16:45] Status: Failed, Error Type: RESP TIMEOUT
[13:16:45] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[13:16:49] [RadarAPI]: Opening Gpio Control Port()
[13:16:49] [RadarAPI]: Status: Passed
[13:16:50] [RadarAPI]: ar1.Disconnect()
[13:16:50] [RadarAPI]: ar1.Calling_ATE_DisconnectTarget()
[13:16:50] [RadarAPI]: ar1.Calling_IsConnected()
[13:16:50] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[13:16:50] [RadarAPI]: Opening Board Control Port()
[13:16:50] [RadarAPI]: Status: Passed
[13:16:51] [RadarAPI]: ar1.FullReset()
[13:16:51] [RadarAPI]: Status: Passed
[13:16:52] [RadarAPI]: Closing Board Control Port()
[13:16:52] [RadarAPI]: Status: Passed
[13:16:52] [RadarAPI]: Closing Gpio Control Port()
[13:16:52] [RadarAPI]: Status: Passed
[13:16:52] [RadarAPI]: ar1.SOPControl(2)
[13:16:52] [RadarAPI]: Status: Passed
[13:16:55] [RadarAPI]: ar1.Connect(4,921600,1000)
[13:16:58] [RadarAPI]: Warning: Connected with baudrate 115200
[13:16:59] [RadarAPI]: Warning: Disconnected existing BaudRate
[13:16:59] [RadarAPI]: Warning: Trying to connect with baudrate 921600
[13:17:01] [RadarAPI]: ar1.Calling_IsConnected()
[13:17:02] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[13:17:02] [RadarAPI]: Status: Passed
[13:17:03] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[13:17:03] [RadarAPI]: Status: Passed
[13:17:03] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[13:17:04] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\radarss\\xwr12xx_xwr14xx_radarss_ES2.0.bin")
[13:17:04] [RadarAPI]: Downloading BSS ROM Legacy Binary..
[13:17:11] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\masterss\\xwr12xx_xwr14xx_masterss_ES2.0.bin")
[13:17:11] [RadarAPI]: Downloading MSS Legacy Binary..
[13:17:17] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[13:17:17] [RadarAPI]: Status: Passed
[13:17:17] MSS power up done async event received!
[13:17:17] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[13:17:19] BSS power up done async event received!
[13:17:19] [RadarAPI]: ar1.RfEnable()
[13:17:19] [RadarAPI]: Status: Passed
[13:17:24] [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 2, 0)
[13:17:24] [RadarAPI]: Status: Passed
[13:17:26] [RadarAPI]: ar1.LPModConfig(0, 0)
[13:17:26] [RadarAPI]: Status: Passed
[13:17:33] [RadarAPI]: ar1.RfSetCalMonFreqTxPowLimitConfig(76, 76, 76, 81, 81, 81, 0, 0, 0)
[13:17:33] [RadarAPI]: Status: Passed
[13:17:41] [RadarAPI]: ar1.RfInit()
[13:17:41] RF Init async event received!
[13:17:41] [RadarAPI]: Time stamp, Temperture: 22380,36; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; RxIQMM Status, Update: 1, 1;
[13:17:41] [RadarAPI]: Status: Passed
[13:17:45] [RadarAPI]: ar1.DataPathConfig(513, 1216644097, 0)
[13:17:45] [RadarAPI]: Status: Passed
[13:17:46] [RadarAPI]: ar1.LvdsClkConfig(1, 1)
[13:17:46] [RadarAPI]: Status: Passed
[13:17:48] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 1, 1, 1, 0, 0)
[13:17:48] [RadarAPI]: Status: Passed
[13:17:54] [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30)
[13:17:54] [RadarAPI]: Status: Passed
[13:17:55] [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 0, 0)
[13:17:55] [RadarAPI]: Status: Passed
[13:17:56] [RadarAPI]: ar1.DisableTestSource(0)
[13:17:56] [RadarAPI]: Status: Passed
[13:17:56] [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 1)
[13:17:56] [RadarAPI]: Status: Passed
[13:17:57] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
[13:17:57] [RadarAPI]: passed
[13:17:59] [RadarAPI]: StatusDCCard Event Registered
[13:17:59] [RadarAPI]: Status: Passed
[13:17:59] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
[13:17:59] [RadarAPI]: SYSTEM_CONNECT_CMD_CODE Async event recieved(9)
[13:17:59] [RadarAPI]: ConnectRFDCCard Status: Passed
[13:17:59] [RadarAPI]: ReadRFDCCarFpgaVersion Status: Passed
[13:17:59] [RadarAPI]: READ_FPGA_VERSION_CMD_CODE event recieved(14)
[13:17:59] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 1, 1, 2, 3, 0)
[13:17:59] [RadarAPI]: Status: Passed
[13:17:59] [RadarAPI]: CONFIG_FPGA_GEN_CMD_CODE Async event recieved(3)
[13:17:59] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[13:17:59] [RadarAPI]: Status: Passed
[13:17:59] [RadarAPI]: CONFIG_PACKET_DATA_CMD_CODE Async event recieved(11)
[13:18:05] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[13:18:05] [RadarAPI]: Status: Passed
[13:18:05] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[13:18:06] [RadarAPI]: ar1.StartFrame()
[13:18:06] [RadarAPI]: STS_LVDS_BUFFER_FULL Async event recieved(9)
[13:18:06] [RadarAPI]: Status: Passed
[13:18:06] Frame start async event received!
[13:18:07] [RadarAPI]: Frame Ended
[13:18:07] Frame End async event received!
[13:18:42] RSTD.ShowLogFile()
[13:19:12] RSTD.ShowVerboseLogFile()
Any ideas on what could be causing this extremely unstable performance?
Thanks,
Sam Bonsor
GM: Constructor
GM: Thu Aug 09 10:40:23 2018
RSTD.Transmit("/Settings")
[10:40:23]
[10:40:23] ### Running Startup script: "C:\ti\mmwave_studio_01_00_00_00\mmWaveStudio\Scripts\Startup.lua" ###
[10:40:23] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[10:40:23] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[10:40:23] Scripter ignored: Attempt to UnBuild() again or before Build.
[10:40:23] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
[10:40:23] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[10:40:23] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[10:40:23] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[10:40:23] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[10:40:23] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[10:40:23] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\RunTime\\SAL.dll")
[10:40:23] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[10:40:23] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[10:40:23] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[10:40:23] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[10:40:23] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[10:40:23] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[10:40:23] RSTD.Transmit("/")
[10:40:23] RSTD.SaveSettings(): Settings saved to "C:\Users\Matthew\AppData\Roaming\RSTD\config.xml"
[10:40:23] RSTD.Build()
[10:40:23] RSTD.SaveSettings(): Settings saved to "C:\Users\Matthew\AppData\Roaming\RSTD\config.xml"
[10:40:23] RSTD.Transmit("/")
[10:40:23] RSTD.AL_Build()
[10:40:23] RSTD.AL_LoadXml()
[10:40:23] RSTD.Transmit("/")
[10:40:23] RSTD.AL_Init()
[10:40:23] RSTD.Clients_Build()
[10:40:23] GM: Init
[10:40:23] GM: Loaded 'C:\ti\mmwave_studio_01_00_00_00\mmWaveStudio\Clients\\LabClient.dll'
[10:40:23] GM: 1 Guest (s) init
[10:40:23] GM: 1 Module(s) init
[10:40:23] GM: 2 Tab (s) init
[10:40:23] RSTD.Client_LoadXml()
[10:40:23] [RadarAPI]: Starting Matlab Engine..
[10:40:26] [RadarAPI]: Matlab Engine Started!
[10:40:29] [RadarAPI]: ar1.LoadSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:40:29] TESTING = false
[10:40:29]
[10:40:29] ***Script completed successfully.***
[10:40:40] [RadarAPI]: Opening Gpio Control Port()
[10:40:40] [RadarAPI]: Status: Passed
[10:40:41] [RadarAPI]: Opening Board Control Port()
[10:40:41] [RadarAPI]: Status: Passed
[10:40:42] [RadarAPI]: ar1.FullReset()
[10:40:42] [RadarAPI]: Status: Passed
[10:40:48] [RadarAPI]: Closing Board Control Port()
[10:40:48] [RadarAPI]: Status: Passed
[10:40:48] [RadarAPI]: Closing Gpio Control Port()
[10:40:48] [RadarAPI]: Status: Passed
[10:40:48] [RadarAPI]: ar1.SOPControl(2)
[10:40:48] [RadarAPI]: Status: Passed
[10:41:01] [RadarAPI]: ar1.Connect(4,921600,1000)
[10:41:03] [RadarAPI]: Warning: Connected with baudrate 115200
[10:41:04] [RadarAPI]: Warning: Disconnected existing BaudRate
[10:41:05] [RadarAPI]: Warning: Trying to connect with baudrate 921600
[10:41:06] [RadarAPI]: ar1.Calling_IsConnected()
[10:41:07] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[10:41:07] [RadarAPI]: Status: Passed
[10:41:08] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[10:41:08] [RadarAPI]: Status: Passed
[10:41:08] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:41:12] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\radarss\\xwr12xx_xwr14xx_radarss_ES2.0.bin")
[10:41:12] [RadarAPI]: Downloading BSS ROM Legacy Binary..
[10:41:38] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\masterss\\xwr12xx_xwr14xx_masterss_ES2.0.bin")
[10:41:38] [RadarAPI]: Downloading MSS Legacy Binary..
[10:42:20] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[10:42:20] [RadarAPI]: Status: Passed
[10:42:20] MSS power up done async event received!
[10:42:20] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:42:24] BSS power up done async event received!
[10:42:24] [RadarAPI]: ar1.RfEnable()
[10:42:24] [RadarAPI]: Status: Passed
[10:42:35] [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 2, 0)
[10:42:35] [RadarAPI]: Status: Passed
[10:42:45] [RadarAPI]: ar1.LPModConfig(0, 0)
[10:42:45] [RadarAPI]: Status: Passed
[10:42:51] [RadarAPI]: ar1.RfSetCalMonFreqTxPowLimitConfig(76, 76, 76, 81, 81, 81, 0, 0, 0)
[10:42:51] [RadarAPI]: Status: Passed
[10:42:55] [RadarAPI]: ar1.RfInit()
[10:42:55] RF Init async event received!
[10:42:55] [RadarAPI]: Time stamp, Temperture: 30925,44; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; RxIQMM Status, Update: 1, 1;
[10:42:55] [RadarAPI]: Status: Passed
[10:43:00] [RadarAPI]: ar1.DataPathConfig(513, 1216644097, 0)
[10:43:00] [RadarAPI]: Status: Passed
[10:43:00] [RadarAPI]: ar1.LvdsClkConfig(1, 1)
[10:43:00] [RadarAPI]: Status: Passed
[10:43:02] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 1, 1, 1, 0, 0)
[10:43:02] [RadarAPI]: Status: Passed
[10:43:21] [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30)
[10:43:21] [RadarAPI]: Status: Passed
[10:43:40] [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 1, 0)
[10:43:40] [RadarAPI]: Status: Passed
[10:43:43] [RadarAPI]: ar1.DisableTestSource(0)
[10:43:43] [RadarAPI]: Status: Passed
[10:43:43] [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 1)
[10:43:43] [RadarAPI]: Status: Passed
[10:43:58] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
[10:43:58] [RadarAPI]: passed
[10:44:02] [RadarAPI]: StatusDCCard Event Registered
[10:44:02] [RadarAPI]: Status: Passed
[10:44:02] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
[10:44:02] [RadarAPI]: SYSTEM_CONNECT_CMD_CODE Async event recieved(9)
[10:44:02] [RadarAPI]: ConnectRFDCCard Status: Passed
[10:44:02] [RadarAPI]: ReadRFDCCarFpgaVersion Status: Passed
[10:44:02] [RadarAPI]: READ_FPGA_VERSION_CMD_CODE event recieved(14)
[10:44:02] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 1, 1, 2, 3, 0)
[10:44:02] [RadarAPI]: Status: Passed
[10:44:02] [RadarAPI]: CONFIG_FPGA_GEN_CMD_CODE Async event recieved(3)
[10:44:02] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[10:44:02] [RadarAPI]: Status: Passed
[10:44:02] [RadarAPI]: CONFIG_PACKET_DATA_CMD_CODE Async event recieved(11)
[10:44:13] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[10:44:13] [RadarAPI]: Status: Passed
[10:44:13] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[10:44:16] [RadarAPI]: ar1.StartFrame()
[10:44:16] [RadarAPI]: Status: Passed
[10:44:16] Frame start async event received!
[10:44:16] [RadarAPI]: Frame Ended
[10:44:16] Frame End async event received!
[10:44:18] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[10:44:18] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[10:44:18] [RadarAPI]: Status: Passed
[10:44:18] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[10:44:22] [RadarAPI]: Packet Reorder Utility Started...please wait...
[10:44:22] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\pktlogfile.txt")
[10:44:27] [RadarAPI]: Packet Reorder Utility process completed!
[10:44:32] Reordering required : NO
[10:44:32] Packet loss : NO
[10:44:32] Number of packets received : 2881
[10:44:32] Number of zero filled packets : 0
[10:44:32] Number of zero filled bytes : 0
[10:44:32] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[10:44:58] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[10:44:58] [RadarAPI]: Status: Passed
[10:44:58] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[10:45:00] [RadarAPI]: ar1.StartFrame()
[10:45:00] [RadarAPI]: Status: Passed
[10:45:00] Frame start async event received!
[10:45:00] [RadarAPI]: Frame Ended
[10:45:00] Frame End async event received!
[10:45:02] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[10:45:02] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[10:45:02] [RadarAPI]: Status: Passed
[10:45:02] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[10:45:07] [RadarAPI]: Packet Reorder Utility Started...please wait...
[10:45:07] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\pktlogfile.txt")
[10:45:12] [RadarAPI]: Packet Reorder Utility process completed!
[10:45:17] Reordering required : NO
[10:45:17] Packet loss : NO
[10:45:17] Number of packets received : 2881
[10:45:17] Number of zero filled packets : 0
[10:45:17] Number of zero filled bytes : 0
[10:45:17] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[10:46:01] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[10:46:01] [RadarAPI]: Status: Passed
[10:46:01] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[10:46:03] [RadarAPI]: ar1.StartFrame()
[10:46:03] [RadarAPI]: Status: Passed
[10:46:03] Frame start async event received!
[10:46:03] Frame End async event received!
[10:46:03] [RadarAPI]: Frame Ended
[10:46:05] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[10:46:05] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[10:46:05] [RadarAPI]: Status: Passed
[10:46:05] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[10:46:06] [RadarAPI]: Packet Reorder Utility Started...please wait...
[10:46:06] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\pktlogfile.txt")
[10:46:11] [RadarAPI]: Packet Reorder Utility process completed!
[10:46:16] Reordering required : NO
[10:46:16] Packet loss : NO
[10:46:16] Number of packets received : 2881
[10:46:16] Number of zero filled packets : 0
[10:46:16] Number of zero filled bytes : 0
[10:46:16] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[10:47:51] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[10:47:51] [RadarAPI]: Status: Passed
[10:47:51] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[10:47:53] [RadarAPI]: ar1.StartFrame()
[10:47:53] [RadarAPI]: Status: Passed
[10:47:53] Frame start async event received!
[10:47:54] Frame End async event received!
[10:47:54] [RadarAPI]: Frame Ended
[10:47:56] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[10:47:56] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[10:47:56] [RadarAPI]: Status: Passed
[10:47:56] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[10:47:59] [RadarAPI]: Packet Reorder Utility Started...please wait...
[10:47:59] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\pktlogfile.txt")
[10:48:04] [RadarAPI]: Packet Reorder Utility process completed!
[10:48:09] Reordering required : NO
[10:48:09] Packet loss : NO
[10:48:09] Number of packets received : 2881
[10:48:09] Number of zero filled packets : 0
[10:48:09] Number of zero filled bytes : 0
[10:48:09] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[10:48:45] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[10:48:45] [RadarAPI]: Status: Passed
[10:48:45] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[10:48:47] [RadarAPI]: ar1.StartFrame()
[10:48:47] [RadarAPI]: Status: Passed
[10:48:47] Frame start async event received!
[10:48:47] [RadarAPI]: Frame Ended
[10:48:48] Frame End async event received!
[10:48:49] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[10:48:49] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[10:48:49] [RadarAPI]: Status: Passed
[10:48:49] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[10:48:51] [RadarAPI]: Packet Reorder Utility Started...please wait...
[10:48:51] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\pktlogfile.txt")
[10:48:56] [RadarAPI]: Packet Reorder Utility process completed!
[10:49:01] Reordering required : NO
[10:49:01] Packet loss : NO
[10:49:01] Number of packets received : 2881
[10:49:01] Number of zero filled packets : 0
[10:49:01] Number of zero filled bytes : 0
[10:49:01] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[10:50:49] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[10:50:49] [RadarAPI]: Status: Passed
[10:50:49] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[10:50:50] [RadarAPI]: ar1.StartFrame()
[10:50:50] [RadarAPI]: Status: Passed
[10:50:50] Frame start async event received!
[10:50:51] Frame End async event received!
[10:50:51] [RadarAPI]: Frame Ended
[10:50:53] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[10:50:53] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[10:50:53] [RadarAPI]: Status: Passed
[10:50:53] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[10:50:54] [RadarAPI]: Packet Reorder Utility Started...please wait...
[10:50:54] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\pktlogfile.txt")
[10:50:59] [RadarAPI]: Packet Reorder Utility process completed!
[10:51:04] Reordering required : NO
[10:51:04] Packet loss : NO
[10:51:04] Number of packets received : 2881
[10:51:04] Number of zero filled packets : 0
[10:51:04] Number of zero filled bytes : 0
[10:51:04] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[10:51:09] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[10:51:09] [RadarAPI]: Status: Passed
[10:51:09] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[10:51:10] [RadarAPI]: ar1.StartFrame()
[10:51:10] [RadarAPI]: Status: Passed
[10:51:10] Frame start async event received!
[10:51:11] [RadarAPI]: Frame Ended
[10:51:11] Frame End async event received!
[10:51:13] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[10:51:13] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[10:51:13] [RadarAPI]: Status: Passed
[10:51:13] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[10:51:14] [RadarAPI]: Packet Reorder Utility Started...please wait...
[10:51:14] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\pktlogfile.txt")
[10:51:19] [RadarAPI]: Packet Reorder Utility process completed!
[10:51:24] Reordering required : NO
[10:51:24] Packet loss : NO
[10:51:24] Number of packets received : 2881
[10:51:24] Number of zero filled packets : 0
[10:51:24] Number of zero filled bytes : 0
[10:51:24] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[10:55:20] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[10:55:20] [RadarAPI]: Status: Passed
[10:55:20] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[10:55:50] [RadarAPI]: STS_NO_LVDS_DATA Async event recieved(0)
[10:56:18] [RadarAPI]: ar1.StartFrame()
[10:56:18] [RadarAPI]: Status: Passed
[10:56:18] Frame start async event received!
[10:56:18] [RadarAPI]: Frame Ended
[10:56:18] Frame End async event received!
[10:56:20] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[10:56:20] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[10:56:20] [RadarAPI]: Status: Passed
[10:56:20] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[10:56:25] [RadarAPI]: Packet Reorder Utility Started...please wait...
[10:56:25] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\pktlogfile.txt")
[10:56:30] [RadarAPI]: Packet Reorder Utility process completed!
[10:56:35] Reordering required : NO
[10:56:35] Packet loss : NO
[10:56:35] Number of packets received : 2881
[10:56:35] Number of zero filled packets : 0
[10:56:35] Number of zero filled bytes : 0
[10:56:35] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[10:57:00] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[10:57:00] [RadarAPI]: Status: Passed
[10:57:00] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[10:57:03] [RadarAPI]: ar1.StartFrame()
[10:57:03] [RadarAPI]: Status: Passed
[10:57:03] Frame start async event received!
[10:57:03] Frame End async event received!
[10:57:03] [RadarAPI]: Frame Ended
[10:57:05] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[10:57:05] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[10:57:05] [RadarAPI]: Status: Passed
[10:57:05] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[10:57:06] [RadarAPI]: Packet Reorder Utility Started...please wait...
[10:57:06] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\pktlogfile.txt")
[10:57:11] [RadarAPI]: Packet Reorder Utility process completed!
[10:57:16] Reordering required : NO
[10:57:16] Packet loss : NO
[10:57:16] Number of packets received : 2881
[10:57:16] Number of zero filled packets : 0
[10:57:16] Number of zero filled bytes : 0
[10:57:16] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[10:58:37] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[10:58:37] [RadarAPI]: Status: Passed
[10:58:37] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[10:58:40] [RadarAPI]: ar1.StartFrame()
[10:58:40] [RadarAPI]: Status: Passed
[10:58:40] Frame start async event received!
[10:58:40] Frame End async event received!
[10:58:40] [RadarAPI]: Frame Ended
[10:58:42] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[10:58:42] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[10:58:42] [RadarAPI]: Status: Passed
[10:58:42] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[10:58:44] [RadarAPI]: Packet Reorder Utility Started...please wait...
[10:58:44] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\pktlogfile.txt")
[10:58:49] [RadarAPI]: Packet Reorder Utility process completed!
[10:58:54] Reordering required : NO
[10:58:54] Packet loss : NO
[10:58:54] Number of packets received : 2881
[10:58:54] Number of zero filled packets : 0
[10:58:54] Number of zero filled bytes : 0
[10:58:54] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[10:59:51] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[10:59:51] [RadarAPI]: Status: Passed
[10:59:51] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[10:59:53] [RadarAPI]: ar1.StartFrame()
[10:59:53] [RadarAPI]: Status: Passed
[10:59:53] Frame start async event received!
[10:59:53] [RadarAPI]: Frame Ended
[10:59:53] Frame End async event received!
[10:59:55] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[10:59:55] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[10:59:55] [RadarAPI]: Status: Passed
[10:59:55] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[10:59:57] [RadarAPI]: Packet Reorder Utility Started...please wait...
[10:59:57] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\pktlogfile.txt")
[11:00:02] [RadarAPI]: Packet Reorder Utility process completed!
[11:00:07] Reordering required : NO
[11:00:07] Packet loss : NO
[11:00:07] Number of packets received : 2881
[11:00:07] Number of zero filled packets : 0
[11:00:07] Number of zero filled bytes : 0
[11:00:07] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[11:03:48] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[11:03:48] [RadarAPI]: Status: Passed
[11:03:48] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[11:03:51] [RadarAPI]: ar1.StartFrame()
[11:03:51] [RadarAPI]: Status: Passed
[11:03:52] Frame start async event received!
[11:03:52] [RadarAPI]: Frame Ended
[11:03:52] Frame End async event received!
[11:03:54] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[11:03:54] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[11:03:54] [RadarAPI]: Status: Passed
[11:03:54] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[11:03:56] [RadarAPI]: Packet Reorder Utility Started...please wait...
[11:03:56] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\pktlogfile.txt")
[11:04:01] [RadarAPI]: Packet Reorder Utility process completed!
[11:04:06] Reordering required : NO
[11:04:06] Packet loss : NO
[11:04:06] Number of packets received : 2881
[11:04:06] Number of zero filled packets : 0
[11:04:06] Number of zero filled bytes : 0
[11:04:06] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[11:07:00] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[11:07:00] [RadarAPI]: Status: Passed
[11:07:00] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[11:07:02] [RadarAPI]: ar1.StartFrame()
[11:07:02] [RadarAPI]: Status: Passed
[11:07:02] Frame start async event received!
[11:07:02] Frame End async event received!
[11:07:02] [RadarAPI]: Frame Ended
[11:07:04] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[11:07:04] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[11:07:04] [RadarAPI]: Status: Passed
[11:07:04] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[11:07:06] [RadarAPI]: Packet Reorder Utility Started...please wait...
[11:07:06] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\pktlogfile.txt")
[11:07:11] [RadarAPI]: Packet Reorder Utility process completed!
[11:07:16] Reordering required : NO
[11:07:16] Packet loss : NO
[11:07:16] Number of packets received : 2881
[11:07:16] Number of zero filled packets : 0
[11:07:16] Number of zero filled bytes : 0
[11:07:16] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[11:10:19] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[11:10:19] [RadarAPI]: Status: Passed
[11:10:19] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[11:10:20] [RadarAPI]: ar1.StartFrame()
[11:10:21] [RadarAPI]: Status: Passed
[11:10:21] Frame start async event received!
[11:10:21] [RadarAPI]: Frame Ended
[11:10:21] Frame End async event received!
[11:10:23] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[11:10:23] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[11:10:23] [RadarAPI]: Status: Passed
[11:10:23] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[11:10:25] [RadarAPI]: Packet Reorder Utility Started...please wait...
[11:10:25] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\pktlogfile.txt")
[11:10:30] [RadarAPI]: Packet Reorder Utility process completed!
[11:10:35] Reordering required : NO
[11:10:35] Packet loss : NO
[11:10:35] Number of packets received : 2881
[11:10:35] Number of zero filled packets : 0
[11:10:35] Number of zero filled bytes : 0
[11:10:35] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[11:11:19] RSTD.ShowLogFile()
[11:11:39] RSTD.ShowVerboseLogFile()
GM: Constructor
GM: Thu Aug 09 10:16:53 2018
RSTD.Transmit("/Settings")
[10:16:53]
[10:16:53] ### Running Startup script: "C:\ti\mmwave_studio_01_00_00_00\mmWaveStudio\Scripts\Startup.lua" ###
[10:16:53] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[10:16:53] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[10:16:53] Scripter ignored: Attempt to UnBuild() again or before Build.
[10:16:53] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
[10:16:53] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[10:16:53] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[10:16:53] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[10:16:53] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[10:16:53] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[10:16:53] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\RunTime\\SAL.dll")
[10:16:53] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[10:16:53] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[10:16:53] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[10:16:53] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[10:16:53] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[10:16:53] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[10:16:53] RSTD.Transmit("/")
[10:16:53] RSTD.SaveSettings(): Settings saved to "C:\Users\Matthew\AppData\Roaming\RSTD\config.xml"
[10:16:53] RSTD.Build()
[10:16:53] RSTD.SaveSettings(): Settings saved to "C:\Users\Matthew\AppData\Roaming\RSTD\config.xml"
[10:16:53] RSTD.Transmit("/")
[10:16:53] RSTD.AL_Build()
[10:16:53] RSTD.AL_LoadXml()
[10:16:53] RSTD.Transmit("/")
[10:16:53] RSTD.AL_Init()
[10:16:53] RSTD.Clients_Build()
[10:16:53] GM: Init
[10:16:53] GM: Loaded 'C:\ti\mmwave_studio_01_00_00_00\mmWaveStudio\Clients\\LabClient.dll'
[10:16:53] GM: 1 Guest (s) init
[10:16:53] GM: 1 Module(s) init
[10:16:53] GM: 2 Tab (s) init
[10:16:53] RSTD.Client_LoadXml()
[10:16:54] [RadarAPI]: Starting Matlab Engine..
[10:16:56] [RadarAPI]: Matlab Engine Started!
[10:17:00] [RadarAPI]: ar1.LoadSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:17:00] TESTING = false
[10:17:00]
[10:17:00] ***Script completed successfully.***
[10:17:27] [RadarAPI]: Opening Gpio Control Port()
[10:17:27] [RadarAPI]: Status: Passed
[10:17:27] [RadarAPI]: Opening Board Control Port()
[10:17:27] [RadarAPI]: Status: Passed
[10:17:28] [RadarAPI]: ar1.FullReset()
[10:17:28] [RadarAPI]: Status: Passed
[10:17:29] [RadarAPI]: Closing Board Control Port()
[10:17:29] [RadarAPI]: Status: Passed
[10:17:29] [RadarAPI]: Closing Gpio Control Port()
[10:17:29] [RadarAPI]: Status: Passed
[10:17:29] [RadarAPI]: ar1.SOPControl(2)
[10:17:29] [RadarAPI]: Status: Passed
[10:17:31] [RadarAPI]: ar1.Connect(4,921600,1000)
[10:17:33] [RadarAPI]: Warning: Connected with baudrate 115200
[10:17:35] [RadarAPI]: Warning: Disconnected existing BaudRate
[10:17:35] [RadarAPI]: Warning: Trying to connect with baudrate 921600
[10:17:36] [RadarAPI]: ar1.Calling_IsConnected()
[10:17:37] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[10:17:37] [RadarAPI]: Status: Passed
[10:17:38] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[10:17:38] [RadarAPI]: Status: Passed
[10:17:38] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:17:43] [RadarAPI]: ar1.ReadRegister(0xffffe210, 0, 31)
[10:17:43] [RadarAPI]: Value : 100000
[10:17:43] [RadarAPI]: ar1.ReadRegister(0xffffe218, 0, 31)
[10:17:43] [RadarAPI]: Value : 12
[10:17:43] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\radarss\\xwr12xx_xwr14xx_radarss_ES2.0.bin")
[10:17:43] [RadarAPI]: Downloading BSS ROM Legacy Binary..
[10:17:49] BSS FW Download Success
[10:17:51] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\masterss\\xwr12xx_xwr14xx_masterss_ES2.0.bin")
[10:17:51] [RadarAPI]: Downloading MSS Legacy Binary..
[10:17:55] MSS FW Download Success
[10:17:57] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[10:17:57] MSS power up done async event received!
[10:17:57] [RadarAPI]: Status: Passed
[10:17:57] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:17:57] Power On Success
[10:17:58] BSS power up done async event received!
[10:17:58] [RadarAPI]: ar1.RfEnable()
[10:17:58] [RadarAPI]: Status: Passed
[10:17:59] RF Enable Success
[10:18:00] [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 1, 0)
[10:18:00] [RadarAPI]: Status: Passed
[10:18:00] ChanNAdcConfig Success
[10:18:01] [RadarAPI]: ar1.LPModConfig(0, 0)
[10:18:01] [RadarAPI]: Status: Passed
[10:18:01] Regualar mode Cfg Success
[10:18:03] [RadarAPI]: ar1.RfInit()
[10:18:04] RF Init async event received!
[10:18:04] [RadarAPI]: Time stamp, Temperture: 5500,42; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; RxIQMM Status, Update: 1, 1;
[10:18:04] [RadarAPI]: Status: Passed
[10:18:04] RfInit Success
[10:18:05] [RadarAPI]: ar1.DataPathConfig(1, 1, 0)
[10:18:05] [RadarAPI]: Status: Passed
[10:18:05] DataPathConfig Success
[10:18:06] [RadarAPI]: ar1.LvdsClkConfig(1, 1)
[10:18:06] [RadarAPI]: Status: Passed
[10:18:06] LvdsClkConfig Success
[10:18:07] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 1, 1, 1, 0, 0)
[10:18:07] [RadarAPI]: Status: Passed
[10:18:07] LVDSLaneConfig Success
[10:18:08] [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30)
[10:18:08] [RadarAPI]: Status: Passed
[10:18:08] ProfileConfig Success
[10:18:09] [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 1, 0)
[10:18:09] [RadarAPI]: Status: Passed
[10:18:09] ChirpConfig Success
[10:18:10] [RadarAPI]: ar1.DisableTestSource(0)
[10:18:10] [RadarAPI]: Status: Passed
[10:18:10] [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 1)
[10:18:10] [RadarAPI]: Status: Passed
[10:18:10] FrameConfig Success
[10:18:11] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
[10:18:11] [RadarAPI]: passed
[10:18:11] SelectCaptureDevice Success
[10:18:12] [RadarAPI]: StatusDCCard Event Registered
[10:18:12] [RadarAPI]: Status: Passed
[10:18:12] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
[10:18:12] [RadarAPI]: Status: Passed
[10:18:12] [RadarAPI]: SYSTEM_CONNECT_CMD_CODE Async event recieved(9)
[10:18:12] [RadarAPI]: ConnectRFDCCard Status: Passed
[10:18:12] [RadarAPI]: Status: Passed
[10:18:12] [RadarAPI]: READ_FPGA_VERSION_CMD_CODE event recieved(14)
[10:18:12] [RadarAPI]: Status: Passed
[10:18:12] CaptureCardConfig_EthInit Success
[10:18:13] [RadarAPI]: ar1.ConfigureRFDCCardMode(1, 1, 1, 2, 3, 0)
[10:18:13] [RadarAPI]: Status: Passed
[10:18:13] [RadarAPI]: CONFIG_FPGA_GEN_CMD_CODE Async event recieved(3)
[10:18:13] CaptureCardConfig_Mode Success
[10:18:14] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[10:18:14] [RadarAPI]: Status: Passed
[10:18:14] [RadarAPI]: CONFIG_PACKET_DATA_CMD_CODE Async event recieved(11)
[10:18:14] CaptureCardConfig_PacketDelay Success
[10:18:15] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", 1)
[10:18:15] [RadarAPI]: Status: Passed
[10:18:15] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[10:18:17] [RadarAPI]: ar1.StartFrame()
[10:18:17] [RadarAPI]: Status: Passed
[10:18:17] Frame start async event received!
[10:18:17] [RadarAPI]: Frame Ended
[10:18:17] Frame End async event received!
[10:18:19] Please wait for a few seconds for Packet reorder utility processing .....!!!!
[10:18:19] [RadarAPI]: Packet Reorder Utility Started...please wait...
[10:18:19] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\pktlogfile.txt")
[10:18:19] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[10:18:19] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[10:18:19] [RadarAPI]: Status: Passed
[10:18:19] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[10:18:24] [RadarAPI]: Packet Reorder Utility process completed!
[10:18:24] Reordering required : NO
[10:18:24] Packet loss : NO
[10:18:24] Number of packets received : 2879
[10:18:24] Number of zero filled packets : 0
[10:18:24] Number of zero filled bytes : 0
[10:18:34] Packet reorder utility processing done.....!!!!
[10:18:34] Please wait for a few seconds for matlab post processing .....!!!!
[10:18:34] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin")
[10:18:44]
[10:18:44] ***Script completed successfully.***
[10:19:05] [RadarAPI]: ar1.PowerOff()
[10:19:05] [RadarAPI]: Status: Passed
[10:19:05] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:19:06] [RadarAPI]: Opening Gpio Control Port()
[10:19:06] [RadarAPI]: Status: Passed
[10:19:06] [RadarAPI]: ar1.Disconnect()
[10:19:06] [RadarAPI]: ar1.Calling_ATE_DisconnectTarget()
[10:19:06] [RadarAPI]: ar1.Calling_IsConnected()
[10:19:06] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:19:06] [RadarAPI]: Opening Board Control Port()
[10:19:06] [RadarAPI]: Status: Passed
[10:19:07] [RadarAPI]: ar1.FullReset()
[10:19:07] [RadarAPI]: Status: Passed
[10:19:08] [RadarAPI]: Closing Board Control Port()
[10:19:08] [RadarAPI]: Status: Passed
[10:19:08] [RadarAPI]: Closing Gpio Control Port()
[10:19:08] [RadarAPI]: Status: Passed
[10:19:08] [RadarAPI]: ar1.SOPControl(2)
[10:19:08] [RadarAPI]: Status: Passed
[10:19:09] [RadarAPI]: ar1.Connect(4,921600,1000)
[10:19:11] [RadarAPI]: Warning: Connected with baudrate 115200
[10:19:12] [RadarAPI]: Warning: Disconnected existing BaudRate
[10:19:13] [RadarAPI]: Warning: Trying to connect with baudrate 921600
[10:19:14] [RadarAPI]: ar1.Calling_IsConnected()
[10:19:15] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[10:19:15] [RadarAPI]: Status: Passed
[10:19:16] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[10:19:16] [RadarAPI]: Status: Passed
[10:19:16] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:19:18] [RadarAPI]: ar1.ReadRegister(0xffffe210, 0, 31)
[10:19:18] [RadarAPI]: Value : 100000
[10:19:18] [RadarAPI]: ar1.ReadRegister(0xffffe218, 0, 31)
[10:19:18] [RadarAPI]: Value : 12
[10:19:18] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\radarss\\xwr12xx_xwr14xx_radarss_ES2.0.bin")
[10:19:18] [RadarAPI]: Downloading BSS ROM Legacy Binary..
[10:19:24] BSS FW Download Success
[10:19:26] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\masterss\\xwr12xx_xwr14xx_masterss_ES2.0.bin")
[10:19:26] [RadarAPI]: Downloading MSS Legacy Binary..
[10:19:30] MSS FW Download Success
[10:19:32] MSS power up done async event received!
[10:19:32] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[10:19:32] [RadarAPI]: Status: Passed
[10:19:32] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:19:32] Power On Success
[10:19:33] BSS power up done async event received!
[10:19:33] [RadarAPI]: ar1.RfEnable()
[10:19:33] [RadarAPI]: Status: Passed
[10:19:34] RF Enable Success
[10:19:35] [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 1, 0)
[10:19:35] [RadarAPI]: Status: Passed
[10:19:35] ChanNAdcConfig Success
[10:19:36] [RadarAPI]: ar1.LPModConfig(0, 0)
[10:19:37] [RadarAPI]: Status: Passed
[10:19:37] Regualar mode Cfg Success
[10:19:39] [RadarAPI]: ar1.RfInit()
[10:19:39] RF Init async event received!
[10:19:39] [RadarAPI]: Time stamp, Temperture: 5421,43; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; RxIQMM Status, Update: 1, 1;
[10:19:39] [RadarAPI]: Status: Passed
[10:19:39] RfInit Success
[10:19:40] [RadarAPI]: ar1.DataPathConfig(1, 1, 0)
[10:19:40] [RadarAPI]: Status: Passed
[10:19:40] DataPathConfig Success
[10:19:41] [RadarAPI]: ar1.LvdsClkConfig(1, 1)
[10:19:41] [RadarAPI]: Status: Passed
[10:19:41] LvdsClkConfig Success
[10:19:42] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 1, 1, 1, 0, 0)
[10:19:42] [RadarAPI]: Status: Passed
[10:19:42] LVDSLaneConfig Success
[10:19:43] [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30)
[10:19:43] [RadarAPI]: Status: Passed
[10:19:43] ProfileConfig Success
[10:19:44] [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 1, 0)
[10:19:44] [RadarAPI]: Status: Passed
[10:19:44] ChirpConfig Success
[10:19:45] [RadarAPI]: ar1.DisableTestSource(0)
[10:19:45] [RadarAPI]: Status: Passed
[10:19:45] [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 1)
[10:19:45] [RadarAPI]: Status: Passed
[10:19:45] FrameConfig Success
[10:19:46] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
[10:19:46] [RadarAPI]: passed
[10:19:46] SelectCaptureDevice Success
[10:19:47] [RadarAPI]: StatusDCCard Event Registered
[10:19:47] [RadarAPI]: Status: Passed
[10:19:47] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
[10:19:47] [RadarAPI]: Status: Passed
[10:19:47] [RadarAPI]: SYSTEM_CONNECT_CMD_CODE Async event recieved(9)
[10:19:47] [RadarAPI]: ConnectRFDCCard Status: Passed
[10:19:47] [RadarAPI]: Status: Passed
[10:19:47] [RadarAPI]: READ_FPGA_VERSION_CMD_CODE event recieved(14)
[10:19:47] [RadarAPI]: Status: Passed
[10:19:47] CaptureCardConfig_EthInit Success
[10:19:48] [RadarAPI]: ar1.ConfigureRFDCCardMode(1, 1, 1, 2, 3, 0)
[10:19:48] [RadarAPI]: Status: Passed
[10:19:48] [RadarAPI]: CONFIG_FPGA_GEN_CMD_CODE Async event recieved(3)
[10:19:48] CaptureCardConfig_Mode Success
[10:19:49] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[10:19:49] [RadarAPI]: Status: Passed
[10:19:49] [RadarAPI]: CONFIG_PACKET_DATA_CMD_CODE Async event recieved(11)
[10:19:49] CaptureCardConfig_PacketDelay Success
[10:19:50] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", 1)
[10:19:50] [RadarAPI]: Status: Passed
[10:19:50] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[10:19:51] [RadarAPI]: ar1.StartFrame()
[10:19:51] [RadarAPI]: Status: Passed
[10:19:51] Frame start async event received!
[10:19:52] [RadarAPI]: Frame Ended
[10:19:52] Frame End async event received!
[10:19:53] Please wait for a few seconds for Packet reorder utility processing .....!!!!
[10:19:53] [RadarAPI]: Packet Reorder Utility Started...please wait...
[10:19:53] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\pktlogfile.txt")
[10:19:54] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[10:19:54] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[10:19:54] [RadarAPI]: Status: Passed
[10:19:54] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[10:19:58] [RadarAPI]: Packet Reorder Utility process completed!
[10:19:58] Reordering required : NO
[10:19:58] Packet loss : NO
[10:19:58] Number of packets received : 2879
[10:19:58] Number of zero filled packets : 0
[10:19:58] Number of zero filled bytes : 0
[10:20:08] Packet reorder utility processing done.....!!!!
[10:20:08] Please wait for a few seconds for matlab post processing .....!!!!
[10:20:08] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin")
[10:20:18]
[10:20:18] ***Script completed successfully.***
[10:21:00] [RadarAPI]: ar1.PowerOff()
[10:21:00] [RadarAPI]: Status: Passed
[10:21:00] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:21:00] [RadarAPI]: Opening Gpio Control Port()
[10:21:00] [RadarAPI]: Status: Passed
[10:21:01] [RadarAPI]: ar1.Disconnect()
[10:21:01] [RadarAPI]: ar1.Calling_ATE_DisconnectTarget()
[10:21:01] [RadarAPI]: ar1.Calling_IsConnected()
[10:21:01] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:21:01] [RadarAPI]: Opening Board Control Port()
[10:21:01] [RadarAPI]: Status: Passed
[10:21:02] [RadarAPI]: ar1.FullReset()
[10:21:02] [RadarAPI]: Status: Passed
[10:21:03] [RadarAPI]: Closing Board Control Port()
[10:21:03] [RadarAPI]: Status: Passed
[10:21:03] [RadarAPI]: Closing Gpio Control Port()
[10:21:03] [RadarAPI]: Status: Passed
[10:21:03] [RadarAPI]: ar1.SOPControl(2)
[10:21:03] [RadarAPI]: Status: Passed
[10:21:04] [RadarAPI]: ar1.Connect(4,921600,1000)
[10:21:07] [RadarAPI]: Warning: Connected with baudrate 115200
[10:21:08] [RadarAPI]: Warning: Disconnected existing BaudRate
[10:21:08] [RadarAPI]: Warning: Trying to connect with baudrate 921600
[10:21:10] [RadarAPI]: ar1.Calling_IsConnected()
[10:21:11] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[10:21:11] [RadarAPI]: Status: Passed
[10:21:12] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[10:21:12] [RadarAPI]: Status: Passed
[10:21:12] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:21:26] [RadarAPI]: ar1.ReadRegister(0xffffe210, 0, 31)
[10:21:26] [RadarAPI]: Value : 100000
[10:21:26] [RadarAPI]: ar1.ReadRegister(0xffffe218, 0, 31)
[10:21:26] [RadarAPI]: Value : 12
[10:21:26] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\radarss\\xwr12xx_xwr14xx_radarss_ES2.0.bin")
[10:21:27] [RadarAPI]: Downloading BSS ROM Legacy Binary..
[10:21:32] BSS FW Download Success
[10:21:34] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\masterss\\xwr12xx_xwr14xx_masterss_ES2.0.bin")
[10:21:34] [RadarAPI]: Downloading MSS Legacy Binary..
[10:21:38] MSS FW Download Success
[10:21:40] MSS power up done async event received!
[10:21:40] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[10:21:40] [RadarAPI]: Status: Passed
[10:21:40] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:21:40] Power On Success
[10:21:41] BSS power up done async event received!
[10:21:41] [RadarAPI]: ar1.RfEnable()
[10:21:41] [RadarAPI]: Status: Passed
[10:21:43] RF Enable Success
[10:21:44] [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 1, 0)
[10:21:44] [RadarAPI]: Status: Passed
[10:21:44] ChanNAdcConfig Success
[10:21:45] [RadarAPI]: ar1.LPModConfig(0, 0)
[10:21:45] [RadarAPI]: Status: Passed
[10:21:45] Regualar mode Cfg Success
[10:21:47] [RadarAPI]: ar1.RfInit()
[10:21:47] RF Init async event received!
[10:21:47] [RadarAPI]: Time stamp, Temperture: 5421,43; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; RxIQMM Status, Update: 1, 1;
[10:21:47] [RadarAPI]: Status: Passed
[10:21:47] RfInit Success
[10:21:48] [RadarAPI]: ar1.DataPathConfig(1, 1, 0)
[10:21:48] [RadarAPI]: Status: Passed
[10:21:48] DataPathConfig Success
[10:21:49] [RadarAPI]: ar1.LvdsClkConfig(1, 1)
[10:21:49] [RadarAPI]: Status: Passed
[10:21:49] LvdsClkConfig Success
[10:21:50] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 1, 1, 1, 0, 0)
[10:21:50] [RadarAPI]: Status: Passed
[10:21:50] LVDSLaneConfig Success
[10:21:51] [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30)
[10:21:51] [RadarAPI]: Status: Passed
[10:21:51] ProfileConfig Success
[10:21:52] [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 1, 0)
[10:21:52] [RadarAPI]: Status: Passed
[10:21:52] ChirpConfig Success
[10:21:53] [RadarAPI]: ar1.DisableTestSource(0)
[10:21:53] [RadarAPI]: Status: Passed
[10:21:53] [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 1)
[10:21:53] [RadarAPI]: Status: Passed
[10:21:53] FrameConfig Success
[10:21:54] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
[10:21:54] [RadarAPI]: passed
[10:21:54] SelectCaptureDevice Success
[10:21:55] [RadarAPI]: StatusDCCard Event Registered
[10:21:55] [RadarAPI]: Status: Passed
[10:21:55] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
[10:21:55] [RadarAPI]: Status: Passed
[10:21:55] [RadarAPI]: SYSTEM_CONNECT_CMD_CODE Async event recieved(9)
[10:21:55] [RadarAPI]: ConnectRFDCCard Status: Passed
[10:21:55] [RadarAPI]: Status: Passed
[10:21:55] [RadarAPI]: READ_FPGA_VERSION_CMD_CODE event recieved(14)
[10:21:55] [RadarAPI]: Status: Passed
[10:21:55] CaptureCardConfig_EthInit Success
[10:21:56] [RadarAPI]: ar1.ConfigureRFDCCardMode(1, 1, 1, 2, 3, 0)
[10:21:56] [RadarAPI]: Status: Passed
[10:21:56] [RadarAPI]: CONFIG_FPGA_GEN_CMD_CODE Async event recieved(3)
[10:21:56] CaptureCardConfig_Mode Success
[10:21:57] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[10:21:57] [RadarAPI]: Status: Passed
[10:21:57] [RadarAPI]: CONFIG_PACKET_DATA_CMD_CODE Async event recieved(11)
[10:21:57] CaptureCardConfig_PacketDelay Success
[10:21:58] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", 1)
[10:21:58] [RadarAPI]: Status: Passed
[10:21:58] [RadarAPI]: RECORD_START_CMD_CODE Async event recieved(5)
[10:21:59] [RadarAPI]: ar1.StartFrame()
[10:22:00] [RadarAPI]: Status: Passed
[10:22:00] Frame start async event received!
[10:22:00] Frame End async event received!
[10:22:00] [RadarAPI]: Frame Ended
[10:22:02] Please wait for a few seconds for Packet reorder utility processing .....!!!!
[10:22:02] [RadarAPI]: Packet Reorder Utility Started...please wait...
[10:22:02] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\pktlogfile.txt")
[10:22:02] [RadarAPI]: STS_RECORD_COMPLETED Async event recieved(8)
[10:22:02] [RadarAPI]: ar1.CaptureCardConfig_StopRecord()
[10:22:02] [RadarAPI]: Status: Passed
[10:22:02] [RadarAPI]: RECORD_STOP_CMD_CODE Async event recieved(6)
[10:22:07] [RadarAPI]: Packet Reorder Utility process completed!
[10:22:07] Reordering required : NO
[10:22:07] Packet loss : NO
[10:22:07] Number of packets received : 2879
[10:22:07] Number of zero filled packets : 0
[10:22:07] Number of zero filled bytes : 0
[10:22:17] Packet reorder utility processing done.....!!!!
[10:22:17] Please wait for a few seconds for matlab post processing .....!!!!
[10:22:17] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin")
[10:22:27]
[10:22:27] ***Script completed successfully.***
[10:31:38] [RadarAPI]: ar1.PowerOff()
[10:31:38] [RadarAPI]: Status: Passed
[10:31:38] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:31:39] [RadarAPI]: Opening Gpio Control Port()
[10:31:39] [RadarAPI]: Status: Passed
[10:31:39] [RadarAPI]: ar1.Disconnect()
[10:31:39] [RadarAPI]: ar1.Calling_ATE_DisconnectTarget()
[10:31:39] [RadarAPI]: ar1.Calling_IsConnected()
[10:31:39] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:31:39] [RadarAPI]: Opening Board Control Port()
[10:31:39] [RadarAPI]: Status: Passed
[10:31:40] [RadarAPI]: ar1.FullReset()
[10:31:40] [RadarAPI]: Status: Passed
[10:31:41] [RadarAPI]: Closing Board Control Port()
[10:31:41] [RadarAPI]: Status: Passed
[10:31:41] [RadarAPI]: Closing Gpio Control Port()
[10:31:41] [RadarAPI]: Status: Passed
[10:31:41] [RadarAPI]: ar1.SOPControl(2)
[10:31:41] [RadarAPI]: Status: Passed
[10:31:43] [RadarAPI]: ar1.Connect(4,921600,1000)
[10:31:46] [RadarAPI]: Warning: Connected with baudrate 115200
[10:31:47] [RadarAPI]: Warning: Disconnected existing BaudRate
[10:31:47] [RadarAPI]: Warning: Trying to connect with baudrate 921600
[10:31:48] [RadarAPI]: ar1.Calling_IsConnected()
[10:31:49] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[10:31:49] [RadarAPI]: Status: Passed
[10:31:50] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[10:31:50] [RadarAPI]: Status: Passed
[10:31:50] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:31:52] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\radarss\\xwr12xx_xwr14xx_radarss_ES2.0.bin")
[10:31:53] [RadarAPI]: Downloading BSS ROM Legacy Binary..
[10:32:06] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\masterss\\xwr12xx_xwr14xx_masterss_ES2.0.bin")
[10:32:06] [RadarAPI]: Downloading MSS Legacy Binary..
[10:32:12] MSS power up done async event received!
[10:32:12] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[10:32:12] [RadarAPI]: Status: Passed
[10:32:12] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:32:14] BSS power up done async event received!
[10:32:14] [RadarAPI]: ar1.RfEnable()
[10:32:14] [RadarAPI]: Status: Passed
[10:32:20] [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 1, 0)
[10:32:20] [RadarAPI]: Status: Passed
[10:32:21] [RadarAPI]: ar1.LPModConfig(0, 0)
[10:32:21] [RadarAPI]: Status: Passed
[10:32:28] [RadarAPI]: ar1.RfSetCalMonFreqTxPowLimitConfig(76, 76, 76, 81, 81, 81, 0, 0, 0)
[10:32:28] [RadarAPI]: Status: Passed
[10:32:37] [RadarAPI]: ar1.RfInit()
[10:32:37] RF Init async event received!
[10:32:37] [RadarAPI]: Time stamp, Temperture: 23155,44; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; RxIQMM Status, Update: 1, 1;
[10:32:37] [RadarAPI]: Status: Passed
[10:32:43] [RadarAPI]: ar1.DataPathConfig(1, 1, 0)
[10:32:43] [RadarAPI]: Status: Passed
[10:32:44] [RadarAPI]: ar1.LvdsClkConfig(1, 1)
[10:32:44] [RadarAPI]: Status: Passed
[10:32:45] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 1, 1, 1, 0, 0)
[10:32:45] [RadarAPI]: Status: Passed
[10:32:49] [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30)
[10:32:49] [RadarAPI]: Status: Passed
[10:32:51] [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 0, 0)
[10:32:51] [RadarAPI]: Status: Passed
[10:32:55] [RadarAPI]: ar1.DisableTestSource(0)
[10:32:55] [RadarAPI]: Status: Passed
[10:32:55] [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 1)
[10:32:55] [RadarAPI]: Status: Passed
[10:32:57] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
[10:32:57] [RadarAPI]: passed
[10:32:59] [RadarAPI]: StatusDCCard Event Registered
[10:32:59] [RadarAPI]: Status: Passed
[10:32:59] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
[10:33:01] ConnectRFDCCard Status: RFDCCARD_UDP_WRITE_ERR
[10:33:01] Ethernet Cable is disconnected Please check.....!!!
[10:33:43] RSTD.ShowLogFile()
[10:34:15] RSTD.ShowVerboseLogFile()
[10:34:57] [RadarAPI]: ar1.PowerOff()
[10:34:57] [RadarAPI]: Status: Passed
[10:34:57] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:34:57] [RadarAPI]: Opening Gpio Control Port()
[10:34:57] [RadarAPI]: Status: Passed
[10:34:58] [RadarAPI]: ar1.Disconnect()
[10:34:58] [RadarAPI]: ar1.Calling_ATE_DisconnectTarget()
[10:34:58] [RadarAPI]: ar1.Calling_IsConnected()
[10:34:58] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:34:58] [RadarAPI]: Opening Board Control Port()
[10:34:58] [RadarAPI]: Status: Passed
[10:34:59] [RadarAPI]: ar1.FullReset()
[10:34:59] [RadarAPI]: Status: Passed
[10:35:00] [RadarAPI]: Closing Board Control Port()
[10:35:00] [RadarAPI]: Status: Passed
[10:35:00] [RadarAPI]: Closing Gpio Control Port()
[10:35:00] [RadarAPI]: Status: Passed
[10:35:00] [RadarAPI]: ar1.SOPControl(2)
[10:35:00] [RadarAPI]: Status: Passed
[10:35:01] [RadarAPI]: ar1.Connect(4,921600,1000)
[10:35:04] [RadarAPI]: Warning: Connected with baudrate 115200
[10:35:05] [RadarAPI]: Warning: Disconnected existing BaudRate
[10:35:05] [RadarAPI]: Warning: Trying to connect with baudrate 921600
[10:35:07] [RadarAPI]: ar1.Calling_IsConnected()
[10:35:08] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[10:35:08] [RadarAPI]: Status: Passed
[10:35:09] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[10:35:09] [RadarAPI]: Status: Passed
[10:35:09] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:35:12] [RadarAPI]: ar1.ReadRegister(0xffffe210, 0, 31)
[10:35:12] [RadarAPI]: Value : 100000
[10:35:12] [RadarAPI]: ar1.ReadRegister(0xffffe218, 0, 31)
[10:35:12] [RadarAPI]: Value : 12
[10:35:12] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\radarss\\xwr12xx_xwr14xx_radarss_ES2.0.bin")
[10:35:12] [RadarAPI]: Downloading BSS ROM Legacy Binary..
[10:35:18] BSS FW Download Success
[10:35:20] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\masterss\\xwr12xx_xwr14xx_masterss_ES2.0.bin")
[10:35:20] [RadarAPI]: Downloading MSS Legacy Binary..
[10:35:23] MSS FW Download Success
[10:35:26] MSS power up done async event received!
[10:35:26] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[10:35:26] [RadarAPI]: Status: Passed
[10:35:26] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[10:35:26] Power On Success
[10:35:27] BSS power up done async event received!
[10:35:27] [RadarAPI]: ar1.RfEnable()
[10:35:27] [RadarAPI]: Status: Passed
[10:35:28] RF Enable Success
[10:35:29] [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 1, 0)
[10:35:29] [RadarAPI]: Status: Passed
[10:35:29] ChanNAdcConfig Success
[10:35:30] [RadarAPI]: ar1.LPModConfig(0, 0)
[10:35:30] [RadarAPI]: Status: Passed
[10:35:30] Regualar mode Cfg Success
[10:35:32] [RadarAPI]: ar1.RfInit()
[10:35:32] RF Init async event received!
[10:35:32] [RadarAPI]: Time stamp, Temperture: 5421,44; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; RxIQMM Status, Update: 1, 1;
[10:35:32] [RadarAPI]: Status: Passed
[10:35:32] RfInit Success
[10:35:33] [RadarAPI]: ar1.DataPathConfig(1, 1, 0)
[10:35:33] [RadarAPI]: Status: Passed
[10:35:33] DataPathConfig Success
[10:35:34] [RadarAPI]: ar1.LvdsClkConfig(1, 1)
[10:35:35] [RadarAPI]: Status: Passed
[10:35:35] LvdsClkConfig Success
[10:35:36] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 1, 1, 1, 0, 0)
[10:35:36] [RadarAPI]: Status: Passed
[10:35:36] LVDSLaneConfig Success
[10:35:37] [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30)
[10:35:37] [RadarAPI]: Status: Passed
[10:35:37] ProfileConfig Success
[10:35:38] [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 1, 0)
[10:35:38] [RadarAPI]: Status: Passed
[10:35:38] ChirpConfig Success
[10:35:39] [RadarAPI]: ar1.DisableTestSource(0)
[10:35:39] [RadarAPI]: Status: Passed
[10:35:39] [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 1)
[10:35:39] [RadarAPI]: Status: Passed
[10:35:39] FrameConfig Success
[10:35:40] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
[10:35:40] [RadarAPI]: passed
[10:35:40] SelectCaptureDevice Success
[10:35:41] [RadarAPI]: StatusDCCard Event Registered
[10:35:41] [RadarAPI]: Status: Passed
[10:35:41] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
[10:35:41] [RadarAPI]: Status: Failed, Error Type: RFDCCARD_OS_ERR
[10:35:43] Ethernet Cable is disconnected Please check.....!!!
[10:35:43] CaptureCardConfig_EthInit failure
[10:35:44] [RadarAPI]: ar1.ConfigureRFDCCardMode(1, 1, 1, 2, 3, 0)
[10:35:44] [RadarAPI]: Status: Failed, Error Type: RFDCCARD_UDP_WRITE_ERR
[10:35:44] CaptureCardConfig_Mode failure
[10:35:45] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[10:35:45] [RadarAPI]: Status: Failed, Error Type: RFDCCARD_UDP_WRITE_ERR
[10:35:45] CaptureCardConfig_PacketDelay failure
[10:35:46] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", 1)
[10:35:46] [RadarAPI]: Status: Failed, Error Type: RFDCCARD_UDP_WRITE_ERR
[10:35:47] [RadarAPI]: ar1.StartFrame()
[10:35:47] [RadarAPI]: Status: Passed
[10:35:47] Frame start async event received!
[10:35:47] [RadarAPI]: Frame Ended
[10:35:47] Frame End async event received!
[10:35:49] Please wait for a few seconds for Packet reorder utility processing .....!!!!
[10:35:49] [RadarAPI]: Packet Reorder Utility Started...please wait...
[10:35:49] [RadarAPI]: ar1.PacketReorderZeroFill("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data_Raw_0.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\pktlogfile.txt")
[10:35:54] [RadarAPI]: Packet Reorder Utility process completed!
[10:36:04] Packet reorder utility processing done.....!!!!
[10:36:04] Please wait for a few seconds for matlab post processing .....!!!!
[10:36:04] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin")
[10:36:04] [RadarAPI]: Error:
[10:36:04]
[10:36:04] ... MWMCR::EvaluateFunction error ...
[10:36:04] 09-Aug-2018 10:36:04: The file C:\ti\mmwave_studio_01_00_00_00\mmWaveStudio\Scripts\..\PostProc\adc_data.bin is empty. Please capture more data.,1,
[10:36:04] Error in => process_adc_data.m at line 52.
[10:36:04]
[10:36:04] ... Matlab M-code Stack Trace ...
[10:36:04] at
[10:36:04] file C:\Users\Matthew\AppData\Local\Temp\Matthew\mcrCache8.5.1\Matlab1\Logging\log_status.m, name log_status, line 32.
[10:36:04] at
[10:36:04] file C:\Users\Matthew\AppData\Local\Temp\Matthew\mcrCache8.5.1\Matlab1\Processing_functions\read_adc_data.m, name read_adc_data, line 28.
[10:36:04] at
[10:36:04] file C:\Users\Matthew\AppData\Local\Temp\Matthew\mcrCache8.5.1\Matlab1\MatlabPostPr\process_adc_data.m, name process_adc_data, line 52.
[10:36:04]
[10:36:04]
[10:36:04] Trace:
[10:36:04] at MathWorks.MATLAB.NET.Utility.MWMCR.EvaluateFunction(String functionName, Int32 numArgsOut, Int32 numArgsIn, MWArray[] argsIn)
[10:36:04] at MathWorks.MATLAB.NET.Utility.MWMCR.EvaluateFunction(Int32 numArgsOut, String functionName, MWArray[] argsIn)
[10:36:04] at MatlabPostProcGui.MatlabPostProcGUIClass.process_adc_data(MWArray adc_file_name, MWArray force_cont_stream_mode)
[10:36:04] at AR1xController.frmAR1Main.iStartMtlabPostProc()
[10:36:11] RSTD.ShowLogFile()
[10:36:14]
[10:36:14] ***Script completed successfully.***
[10:36:25] RSTD.ShowVerboseLogFile()
GM: Constructor
GM: Thu Aug 09 09:47:45 2018
RSTD.Transmit("/Settings")
[09:47:46]
[09:47:46] ### Running Startup script: "C:\ti\mmwave_studio_01_00_00_00\mmWaveStudio\Scripts\Startup.lua" ###
[09:47:46] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[09:47:46] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[09:47:46] Scripter ignored: Attempt to UnBuild() again or before Build.
[09:47:46] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
[09:47:46] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[09:47:46] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[09:47:46] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[09:47:46] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[09:47:46] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[09:47:46] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\RunTime\\SAL.dll")
[09:47:46] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[09:47:46] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[09:47:46] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[09:47:46] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[09:47:46] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[09:47:46] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[09:47:46] RSTD.Transmit("/")
[09:47:46] RSTD.SaveSettings(): Settings saved to "C:\Users\Matthew\AppData\Roaming\RSTD\config.xml"
[09:47:46] RSTD.Build()
[09:47:46] RSTD.SaveSettings(): Settings saved to "C:\Users\Matthew\AppData\Roaming\RSTD\config.xml"
[09:47:46] RSTD.Transmit("/")
[09:47:46] RSTD.AL_Build()
[09:47:46] RSTD.AL_LoadXml()
[09:47:46] RSTD.Transmit("/")
[09:47:46] RSTD.AL_Init()
[09:47:46] RSTD.Clients_Build()
[09:47:46] GM: Init
[09:47:46] GM: Loaded 'C:\ti\mmwave_studio_01_00_00_00\mmWaveStudio\Clients\\LabClient.dll'
[09:47:46] GM: 1 Guest (s) init
[09:47:46] GM: 1 Module(s) init
[09:47:46] GM: 2 Tab (s) init
[09:47:46] RSTD.Client_LoadXml()
[09:47:46] [RadarAPI]: Starting Matlab Engine..
[09:48:42] [RadarAPI]: Matlab Engine Started!
[09:48:47] [RadarAPI]: ar1.LoadSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[09:48:48] TESTING = false
[09:48:48]
[09:48:48] ***Script completed successfully.***
[09:51:32] [RadarAPI]: Opening Gpio Control Port()
[09:51:32] [RadarAPI]: Status: Passed
[09:51:32] [RadarAPI]: Opening Board Control Port()
[09:51:32] [RadarAPI]: Status: Passed
[09:51:33] [RadarAPI]: ar1.FullReset()
[09:51:33] [RadarAPI]: Status: Passed
[09:51:34] [RadarAPI]: Closing Board Control Port()
[09:51:34] [RadarAPI]: Status: Passed
[09:51:34] [RadarAPI]: Closing Gpio Control Port()
[09:51:34] [RadarAPI]: Status: Passed
[09:51:34] [RadarAPI]: ar1.SOPControl(2)
[09:51:34] [RadarAPI]: Status: Passed
[09:51:58] [RadarAPI]: ar1.Connect(4,921600,1000)
[09:52:00] [RadarAPI]: Warning: Connected with baudrate 115200
[09:52:01] [RadarAPI]: Warning: Disconnected existing BaudRate
[09:52:01] [RadarAPI]: Warning: Trying to connect with baudrate 921600
[09:52:03] [RadarAPI]: ar1.Calling_IsConnected()
[09:52:04] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[09:52:04] [RadarAPI]: Status: Passed
[09:52:05] [RadarAPI]: ar1.SelectChipVersion("XWR1243")
[09:52:05] [RadarAPI]: Status: Passed
[09:52:05] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[09:52:09] [RadarAPI]: ar1.ReadRegister(0xffffe210, 0, 31)
[09:52:09] [RadarAPI]: Value : 100000
[09:52:10] [RadarAPI]: ar1.ReadRegister(0xffffe218, 0, 31)
[09:52:10] [RadarAPI]: Value : 12
[09:52:10] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\radarss\\xwr12xx_xwr14xx_radarss_ES2.0.bin")
[09:52:10] [RadarAPI]: Downloading BSS ROM Legacy Binary..
[09:52:15] BSS FW Download Success
[09:52:17] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\masterss\\xwr12xx_xwr14xx_masterss_ES2.0.bin")
[09:52:18] [RadarAPI]: Downloading MSS Legacy Binary..
[09:52:21] MSS FW Download Success
[09:52:46] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[09:52:46] Status: Failed, Error Type: RESP TIMEOUT
[09:52:46] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[09:52:46] Power On failure
[09:52:47] [RadarAPI]: ar1.RfEnable()
[09:52:47] Status: Failed, Error Type: INVALID INPUT
[09:52:47] [RadarAPI]: Error Occurred in Port open close
[09:52:48] RF Enable failure
[09:52:49] [RadarAPI]: ar1.Disconnect()
[09:52:49] [RadarAPI]: ar1.Calling_ATE_DisconnectTarget()
[09:52:49] [RadarAPI]: Debug Port Disconnected!
[09:52:49] [RadarAPI]: ar1.PowerOn(1, 0, 1, 4)
[09:52:49] Status: Failed, Error Type: PROTOCOL ERROR
[09:52:49] [RadarAPI]: ar1.SaveSettings('C:\Users\Matthew\AppData\Roaming\RSTD\ar1gui.ini')
[09:52:49] [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 1, 0)
[09:52:49] Status: Failed, Error Type: INVALID INPUT
[09:52:49] ChanNAdcConfig failure
[09:52:50] [RadarAPI]: ar1.LPModConfig(0, 0)
[09:52:50] [RadarAPI]: Status: Failed, Error Type: INVALID INPUT
[09:52:50] [RadarAPI]: Error Occurred in Port open close
[09:52:50] Regualar mode Cfg failure
[09:52:52] [RadarAPI]: ar1.RfInit()
[09:52:59]
[09:52:59] *** Script aborted by user ***
[09:53:06] RSTD.ShowLogFile()