This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT8241: Higher dynamic range for the illumination power

Part Number: OPT8241
Other Parts Discussed in Thread: TPS2559

Hi,

I need high dynamic range for the illumination power, but it seems that I can control only from 48% to 100% of maximum illumination power.

Is there any solution to increase dynamic range for the illumination power like from 10% to 100%?

Thanks.