Other Parts Discussed in Thread: IWR1443,
Hi Experts,
By referring to IWR1443EVM TRM and from below points its clear that IWR1443 is CSI & not DSI.
- IWR1443EVM supports only MIPI-CSI2
- There is no reference to DSI in entire TRM.
- DSI requires 3 Uni-directional data lanes & 1 bi-directional data command lane. But in CSI2 all 4 data lanes are Uni-directional.
IWR1443EVM TRM mentions all 4 data lanes are Uni-directional (refer 13.4.1)
But I have below queries which contractics the above points. So Please answer below queries -
1 - There is no information about command mode in MIPI CSI specification. But in MIPI DSI specification there is description about command mode and its supported.
IWR1443EVM also support only command mode. So IWR1443EVM using CSI or DSI ? Please confirm ?
2 - By referring section 13.4.2.10.4 "Display Timing Configuration", this seems to be DSI and not CSI . Please confirm ?
3 - By referring section Table 13-158. "CSI2_IRQSTATUS Register Field Descriptions (continued), (Register Bit 5)"
IWR1443Evm should be interface with DSI & not CSI. Please confirm ?
4 - From refering section 13.4.4.6 CSI2_CTRL Register (Offset = 40h) [reset = 100h], again it looks like DSI and not CSI. Please confirm ?
5 - If IWR1443EVM using DSI, can we interface the other end of the custom cable to CSI of another host processor ?? What is TI recommendation ??
6 - Please confirm whether IWR1443EVM is really using CSI or DSI ??
Waiting for your reply. Thanks in advance.
Regards
Gajanan