Hi SIr
We saw the description from the spec as below
6.2 Individual Transmitter Binary Phase Modulation (BPM)
TI’s radar device allows each of the transmitter outputs to be modulated by a phase of 0° or 180°.
This allows usage of multiple transmitters simultaneously by using mutually uncorrelated binary codes.
hence,improving the effective SNR.
The phase configuration is done by the “rlSetBpmChirpConfig” API. For details on BPM and MIMO radar,
see MIMO Radar .
Q1: We want to know that RF Front End could decode mutually uncorrelated binary codes according to the TX setting ?
Q2:Since each receive antenna will have received echo with different delays.
After the decoding, how I can get the information about the delays? It is better if I can know how it decodes. Is it doing decode the
echo on DSP or other than RF Front?
thanks for reply.
BR
Yimin