Other Parts Discussed in Thread: AWR1642, UNIFLASH, MMWAVE-SDK
I am attempting to run the Demo Visualizer example and I cannot get Demo visualizer to connect to the AWR1642 BOOST EVM board. I've tried using the web app on Chrome/Firefox on Linux and Win10 and using the offline Demo Visualizer. I believe I've set up the COM ports and TTYACM0 ports correctly. I even downloaded minicom in Ubuntu, connected it to ttyACM0 and pressed 'enter' as suggested in another post and it returned "mmwDemo :/>" indicating the demo was flashed properly. I also tried reflashing the Demo binary with Uniflash.
Here is a screen shot of the connection issue:
Sometimes this area just says "Connecting to Target" but never connects.
In the serial port configuration page, the program can select the correct ports.
What am I missing here? What steps should I take to troubleshoot this issue.