Other Parts Discussed in Thread: IWR1443BOOST
Hi,
I use DCA1000EVM and IWR1443BOOST.
When data is collected with the following parameters,
the frame upper limit is 300 on the playback screen.
No of Frame:0
No of Chirp:128
Bin Data 0:1,048,576kb(It got full with about 2 minutes)
Bin Data 1:1,048,576kb
Bin Data 2: 188,928kb(Stop in the middle)
Post Prock Frame:300(Data 0,1,and 2)
Post Prock Chirp:128
Does it play only the first 300?
Or is it thinning out the data to 300 frames?
Regards,
user5205609