This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: VIOIN at 1.8V

Part Number: AWR1243
Other Parts Discussed in Thread: AWR1642

Hi,

a customer is trying to see if they can run the CMOS I/O at 1.8v for the AWR1243. The pin description for the VIOIN pin on R13 shows that it can be either 1.8V or 3.3V. The datasheet however only shows MIN/NOM/MAX specs for 3.3V on this pin. What are the 1.8V specs?

Also what CMOS I/O is operating on the VIOIN voltage exactly?

Thanks!

--Gunter