This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-GASEVM: a problem about headware on TDC1000-GASEVM

Part Number: TDC1000-GASEVM

Hello,

When I test the TDC1000-GASEVM to set the green board to HV, the 5 pin of U2 and U3 on the green board has signal, but the single floweg throgh the resistance R12 and R22 is diapperred. Why?In addition, RX will also output a 3~5V signal  similar to pulse  , is that normal?