Other Parts Discussed in Thread: AWR1243
Hello experts,
Recently, I started looking into IWR1443 and want to interface with another processor with MIPI-CSI2 interface.
While browsing through many posts on this forum, one common thing I have noticed is, TI recommends using converter such as FPD link for interfacing IWR & TDA3x via CSI2. Since TDA3x & IWR1443/AWR1243 are CSI2 compliant devices, we should be able to interface them directly without any additional components/converters/IC's in between.
Is there any specific reason/known issues in interfacing it directly ?
Here I found few recommendations from TI:
- The combination of AWR1243BOOST (IWR1443BOOST) and TDA3x EVM to read the ADC data over the CSI is not easy because it requires three additional boards, i.e. MMWAVE-DEVPACK, AR1243 DIB EVM-1 and AR1243 VAB EVM-1. Besides, for DIB and VAB the board design data is only available.
https://e2e.ti.com/support/sensor/mmwave_sensors/f/1023/t/619887?IWR1443-Direct-recording-of-raw-ADC-data-over-CSI - Another link talks about 'TDA3xx EVM + DIB + VAB + AWR12 Booster Pack'
- TDA3x Processor SDK documentation also talks in the same line.
Ref: Processor SDK – Radar (v03.04) User Guide - Section 2.3
Appreciate your help.
Thanks