hello to the whole team
I have some questions to ask about using the tdc100-tdc7200 board to use as a liquid flow meter
1) in the software TDC100-TDC7200 EVM is present only the tank part, and even check "flow mode" does not appear the instrument for measuring the flow rate, in your videos instead you see, there is a specific version of the software? my version is the 2.01 GUI revision 1.2.7.1
2) my application would require 45 ° clamp-on sensors, in all the flow meters of this type requires the setting of the pipe material and the thickness, my idea to avoid errors on the TOF count is to calculate the time of ultrasound crossing that then subtracted from the total TOF could be a good idea?
Thanks for your answers