This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC2080: Some questions

Part Number: HDC2080
Other Parts Discussed in Thread: HDC2010

Hi Sirs,

Sorry to bother you.

We are survey Humidity between Si7021-A20 and 2080

On 2080. some spec need check, could you help it?

  1. The process flow to prevent the condensation (5’C- -40’C environment for cold-chain application)
  2. The effects of thermal sensor after internal heater on.
  3. The mechanical design for humidity.
  4. How to assess the power consumption?

I can’t get the number from below table from the spec.

-       0.55uA 11-bit Temp. / 11-bit RH / per second sensing.

-       However, the table shows:

 650uA for RH measurement with 400uS conversion time,

and 550uA for temp. measurement with 350uA conversion time,

650uA*0.4s + 550uA*0.35s =452uA >> 0.55uA, not even include quiescent current.

    1. The process flow to prevent the condensation (5’C- -40’C environment for cold-chain application)
      1. Briefly turn on the heater to prevent and condensation or build up of water on the humidity sensor.
    2. The effects of thermal sensor after internal heater on.90mA of current to heat the device, and will heat up the sensor as
      1. The heater pulls ~90mA of current to heat the device, and will heat up the sensor as a result.  To record accurate temperature information you will need to allow the sensor to cool to ambient conditions.
    3. The mechanical design for humidity.
      1. Do you mean an example of an enclosed casing, or do you mean packaging information?
    4. How to assess the power consumption?
      1. Do you mean you need the ability to track the amount of power the device is consuming?

    Regarding the question about the RH Supply Current of 650uA, please note the (1) footnote next to this parameter description. (1) I2C read/write communication and pull up resistors current through SCL, SDA not included.  This footnote explains that most of this current is a result of I2C communication. During writes/read current is being sourced/sunk through these pullup resistors.  This current value does not reflect the amount of current consumption when the part is idle or in sleep mode.

    Best Regards,

    Matt

  • Hi Sirs,

    Please refer our update as below

    Briefly turn on the heater to prevent and condensation or buildup of water on the humidity sensor.

    We need the flow for the reference, like this:

    -       turn on the sensor power or wake up the sensor,

    -       heater ON for 1sec to hydrate the cave, OFF for 10sec to cool down,

    -       convert and read the RH & TEMP data,

    -       go to sleep or sensor power off.

    The heater pulls ~90mA of current to heat the device, and will heat up the sensor as a result.  To record accurate temperature information you will need to allow the sensor to cool to ambient conditions.

    what’s the recommended time on the heater ON and OFF?

     

    Do you mean an example of an enclosed casing, or do you mean packaging information?

     Enclosure casing design per the talk in the meeting yesterday,

    by the way, is the chip working under high level humidity, even few condensation on the pins of the sensor chip?

     

    Do you mean you need the ability to track the amount of power the device is consuming?

    Yes, I need the methodology to assess the power consumptions and how to derive the 0.55uA per second reading.  I’m a bit confused of the IDD supply current on the spec

    .

    Regarding the question about the RH Supply Current of 650uA, please note the (1) footnote next to this parameter description. (1) I2C read/write communication and pull up resistors current through SCL, SDA not included.  This footnote explains that most of this current is a result of I2C communication. During writes/read current is being sourced/sunk through these pullup resistors.  This current value does not reflect the amount of current consumption when the part is idle or in sleep mode.

  • Hi Shu-Cheng LIN,

    You will need to evaluate the heater in your end application or product to determine the duration that you may require for activation. I'll update you on whether there are methodologies to assess the power consumption of the device. I believe I can probably find an equation that will suite your request.

    Best Regards,
    Matt
  • Hi Shu-Cheng Lin,

    For the calculation of Average Current Consumption:

    HDC2010 average current consumption is function of selected parameters:
    • Resolution;
    • Output data rate;
    Average current consumption takes in account the following specifications:
    • Current consumption during conversion;
    • Data conversion duration (RHCTand TEMPCT);
    • Current consumption in stand-by (IDD-SLEEP)
    Average current calculation


    Average current = {[(H_Conv_Time* H_Conv_Cur) + (T_Conv_Time* T_Conve_Corr )]+[(ODR-(T_Conv_Time +
    T_Conve_Corr ))* Sleep )]}/ODR
    Example:
    • Resolution = 11bit for both Humidity and Temperature
    • Output Data Rate: ODR = 1Hz (1sec = 1000000us)
    • Humidity conversion time: H_Conv_Time = 400us (for 11 bit resolution)
    • Temperature conversion time: T_Conv_Time = 350 us (for 11 bit resolution)
    • Humidity conversion current consumption: H_Conv_Cur = 650uA
    • Temperature conversion current consumption: T_Conve_Corr = 550uA
    • Sleep current: Sleep = 0.05uA
    Average current = {[(400us*650uA)+(350us*550uA)]+[(1000000us-(400us+350us))*0.05uA)]}/1000000us =
    0.502uA

    If you have any questions please let me know.

    Best Regards,
    Matt