Other Parts Discussed in Thread: MMWAVE-SDK
Tool/software: Code Composer Studio
I am trying to run "Vital Signs Demo lab" on IWR1443boost. Everything goes smoothly until I run the GUI Matlab runtime. No response on the GUI screen.
The error message as follows. Please help!!!!
Debug: CLI is operational
Debug: Start ADCBuf driver dataFormat=0, sampleSwap=1, interleave=0, chirpThreshold=1
Error: HWA_configParamSet(4) returned -2801 in function HWAutil_configVitalSignsFFT
Exception occurred in ThreadType_Task.
Task handle: 0x8003778.
Task stack base: 0x80037c8.
Task stack size: 0xc00.
R0 = 0x5105fffc R8 = 0x080082c4
R1 = 0x0000fbff R9 = 0x080082c4
R2 = 0x08004010 R10 = 0x510217d0
R3 = 0x080088c8 R11 = 0xffffffff
R4 = 0x00000000 R12 = 0x00000000
R5 = 0x00000000 SP(R13) = 0x08003fc0
R6 = 0x94785cdd LR(R14) = 0x000003ff
R7 = 0x00000000 PC(R15) = 0x0000afa4
PSR = 0x200c019f
DFSR = 0x00000008 IFSR = 0x00000000
DFAR = 0x51060000 IFAR = 0x00000000
{module#40}: line 205: error {id:0x180000, args:[0xafa4, 0x3ff]}
xdc.runtime.Error.raise: terminating execution