Tool/software: WEBENCH® Design Tools
I'm using mmWave Studio for Rx Monitoring testing. I got the test report, MonitoringReport.txt. The contents are as follows:
"
[09:56:51] MonitoringReportHeader: 0, 40
[09:56:51] RxMixerInputPowerMonitoring: 13, 0, 0, 0, 7, 0, 0, 356442
[09:56:51] MonitoringReportHeader: 1, 40
[09:56:51] RxMixerInputPowerMonitoring: 11, 0, 0, 0, 0, 7, 0, 356482
[09:56:51] MonitoringReportHeader: 2, 41
[09:56:51] RxMixerInputPowerMonitoring: 12, 0, 0, 7, 28, 0, 0, 356522
[09:56:51] MonitoringReportHeader: 3, 41
[09:56:51] RxMixerInputPowerMonitoring: 13, 0, 0, 0, 14, 0, 0, 356562
[09:56:51] MonitoringReportHeader: 4, 41
[09:56:51] RxMixerInputPowerMonitoring: 11, 0, 0, 0, 0, 14, 0, 356602
[09:56:51] MonitoringReportHeader: 5, 41
[09:56:51] RxMixerInputPowerMonitoring: 11, 0, 0, 0, 0, 7, 0, 356642
[09:56:51] MonitoringReportHeader: 6, 42
[09:56:51] RxMixerInputPowerMonitoring: 15, 0, 0, 0, 0, 0, 0, 356682
[09:56:51] MonitoringReportHeader: 7, 42
[09:56:51] RxMixerInputPowerMonitoring: 15, 0, 0, 0, 0, 0, 0, 356722
"
We know that the rlMonRxMixrInPwrRep in mmwave_sdk_01_02_00_05 is as follows:
typedef struct rlMonRxMixrInPwrRep
{
rlUInt16_t statusFlags;
rlUInt16_t errorCode;
rlUInt32_t rxMixInVolt;
rlUInt32_t reserved0;
rlUInt32_t timeStamp;
}rlMonRxMixrInPwrRep_t;
Question:
what is the information in the report, which number represents the rxMixInVolt? or
rxMixInVolt = ?