Using IWR1642BOOST chip rev 502AC, which I believe makes this an ESR 2.0 board even though it has no sticker.
Using mmwave_sdk_02_00_00_04 demo visualizer 2.0.0.
Using mmwave_industrial_toolbox_2_5_1\labs\lab0013_traffic_monitoring_16xx\chirp_configs\*
I believe this is the correct set of software for this board; please advise if not.
The chirp configs do not load in the demo visualizer. Some commands have an invalid number of arguments, and some required commands are missing. I attempted to address these issues by replacing invalid commands with known-good commands from the demo's included configurations; however, I do not know if the values support the profile and chirp configs specified in the lab. My attempt below:
mmwDemo:/>sensorStop Done mmwDemo:/>sensorStop Done mmwDemo:/>flushCfg Done mmwDemo:/>dfeDataOutputMode 1 Done mmwDemo:/>channelCfg 15 1 0 Done mmwDemo:/>adcCfg 2 1 Done mmwDemo:/>%adcbufCfg 0 1 1 1 - error in demo, must be set to -1 Skipped mmwDemo:/>adcbufCfg -1 0 0 1 0 Done mmwDemo:/>profileCfg 0 76 2 5 52.62 0 0 4.007 1 256 5490 0 0 48 Done mmwDemo:/>chirpCfg 0 0 0 0 0 0 0 1 Done mmwDemo:/>frameCfg 0 0 118 0 50 1 0 Done mmwDemo:/>lowPower 0 1 Done mmwDemo:/>%guiMonitor 1 0 0 0 - error in demo, invalid number of args Skipped mmwDemo:/>guiMonitor -1 1 1 0 0 0 1 Done mmwDemo:/>%cfarCfg 4 12 2 16 8 4 0 63 63 0 1 - error in demo, invalid number of args Skipped mmwDemo:/>cfarCfg -1 0 0 8 4 4 0 6000 Done mmwDemo:/>%doaCfg 3 0 1047 3 600 10 100 - error in demo, unrecognized command Skipped mmwDemo:/>%trackingCfg 1 1 250 20 189 330 50 90 - error, unrecognized command Skipped mmwDemo:/>compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 Done mmwDemo:/>peakGrouping -1 1 1 1 1 255 Done mmwDemo:/>multiObjBeamForming -1 1 0.5 Done mmwDemo:/>clutterRemoval -1 0 Done mmwDemo:/>calibDcRangeSig -1 0 -5 8 256 Done mmwDemo:/>extendedMaxVelocity -1 0 Done mmwDemo:/>bpmCfg -1 0 0 1 Done mmwDemo:/>lvdsStreamCfg -1 0 0 0 Done mmwDemo:/>nearFieldCfg -1 0 0 0 Done mmwDemo:/>measureRangeBiasAndRxChanPhase 0 1.5 0.2 Done mmwDemo:/>CQRxSatMonitor 0 3 4 127 0 Done mmwDemo:/>CQSigImgMonitor 0 127 4 Done mmwDemo:/>analogMonitor 1 1 Done mmwDemo:/>sensorStart Debug: Init Calibration Status = 0x7fe DSS Exception: dss/dss_main.c, line 2005.
mmwDemo:/>sensorStop Done mmwDemo:/>sensorStop Done mmwDemo:/>flushCfg Done mmwDemo:/>dfeDataOutputMode 1 Done mmwDemo:/>channelCfg 15 1 0 Done mmwDemo:/>adcCfg 2 1 Done mmwDemo:/>%adcbufCfg 0 1 1 1 - error in demo, must be set to -1 Skipped mmwDemo:/>adcbufCfg -1 0 0 1 0 Done mmwDemo:/>profileCfg 0 76 2 5 52.62 0 0 4.007 1 256 5490 0 0 48 Done mmwDemo:/>chirpCfg 0 0 0 0 0 0 0 1 Done mmwDemo:/>frameCfg 0 0 118 0 50 1 0 Done mmwDemo:/>lowPower 0 1 Done mmwDemo:/>%guiMonitor 1 0 0 0 - error in demo, invalid number of args Skipped mmwDemo:/>guiMonitor -1 1 1 0 0 0 1 Done mmwDemo:/>%cfarCfg 4 12 2 16 8 4 0 63 63 0 1 - error in demo, invalid number of args Skipped mmwDemo:/>cfarCfg -1 0 0 8 4 4 0 6000 Done mmwDemo:/>%doaCfg 3 0 1047 3 600 10 100 - error in demo, unrecognized command Skipped mmwDemo:/>%trackingCfg 1 1 250 20 189 330 50 90 - error, unrecognized command Skipped mmwDemo:/>compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 Done mmwDemo:/>peakGrouping -1 1 1 1 1 255 Done mmwDemo:/>multiObjBeamForming -1 1 0.5 Done mmwDemo:/>clutterRemoval -1 0 Done mmwDemo:/>calibDcRangeSig -1 0 -5 8 256 Done mmwDemo:/>extendedMaxVelocity -1 0 Done mmwDemo:/>bpmCfg -1 0 0 1 Done mmwDemo:/>lvdsStreamCfg -1 0 0 0 Done mmwDemo:/>nearFieldCfg -1 0 0 0 Done mmwDemo:/>measureRangeBiasAndRxChanPhase 0 1.5 0.2 Done mmwDemo:/>CQRxSatMonitor 0 3 4 127 0 Done mmwDemo:/>CQSigImgMonitor 0 127 4 Done mmwDemo:/>analogMonitor 1 1 Done mmwDemo:/>sensorStart Debug: Init Calibration Status = 0x7fe DSS Exception: dss/dss_main.c, line 2005.