Part Number: PGA900EVM
Dear Sir or Madame,
I have a PGA900EVM and would like to connect an external bridge instead of the built in bridge. My idea would be to open Jumpers J1 - J3 and to connect my own bridge there. See Screenshot from EVM User Guide (p. 4):
My Questions:
1) Is it possible to connect an external bridge to the EVM? If yes, where to connect VBRGN of the external bridge? To Test Point 37 of the module?
2) How can I realise the calibration of the system for a 4 - 20 mA output signal, is there somewhere a step by step description? I couldn't find one in the documentation (I went through PGAxxxEVM-034 User Guide and PGA900 Data sheet)
3) Same as 2) but for 0 - 10 V output
Thanks in advance and best regards
Tobias