Other Parts Discussed in Thread: UNIFLASH, IWR1642
Hello together,
I am using the IWR1443 on my own PCB design. My PCB has a JTAG interface ( MIPI 14-Pin JTAG Adapter) connected to the IWR device. Not having the XDS110 anymore. I use the Sprectrum Digital XDS560V2 STM Emulator with the JTAG adapters. In the section software features of the XDS560V2 is mentioned that Uniflash is featured! But I wasn't able to flash yet. I use the latest version of Uniflash ( V4.2.2 ). The SOP jumpers are 101 for flashing mode. The Flash is the S25FL132K ( Spansion). This would be the first time flashing the memory devide. Uniflash is not finding any device or a COM-Port with the XDS560V2 connected.
My Questions:
1) Is it possible to flash the device with the XDS560V2? If yes, how I'm doing it exactly?
2) Is there any other possibility to flash, like RS232 or CCS? I would be able to connect the RS232-TX & -RX pins of IWR1443 for communicating over UART.
Thanks and regards,
Jan