I am using AWR1642+TSW1400 to capture ADC data.
i have 2 questions about mmwave studdio config.
1/ in SecsorConfig tab, there is a VCO select option.I can select VCO1 or VCO2.
i want to confirm: does VCO1 means 76-78GHz and VCO2 means 77-81GHz?
2/ bandwidth of VCO1 is 2GHz, and VCO2 is 4GHz。
Does it mean i can only congfig a chirp with max 76-78GHz or 77-81GHz, i can not config 76-79/80/81GHz?