Other Parts Discussed in Thread: FDC2214
Hello,
I would like to confirm 3 issues:
the resolution in Farads of the chip. In máximum ratings I see a max capacity of 250nF. Is the teorical resolution then 250nF/2^28=0.93fF?
the mínimum capacity posible to measure. If we use the recomended C in parallel of 33pF and L of 18uH, then the max frecuency of oscilation in sensor side is 6,5Mhz. Any capacity to be measured will be added to this 33pF and will decrease the frecuency. The mínimum capacity to be measured is the resolution then? The max is 250nF?
Capacity variation for a 1500 counts variation. If we use the recomended C in parallel of 33pF and L of 18uH, and Fref=40MHz, and CHx_FIN_SEL=1, then are the capacity values like this?:
• DATAx = 30000000 => 3.74182168049954E-11F --> 37.4182pF
• DATAx = 30001500 => 3.74111755114163E-11F --> 37.4111pF
thanks in advance,
Miguel