This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: BIT-file for FPGA with config over Ethernet

Part Number: DCA1000EVM
Other Parts Discussed in Thread: AWR1243BOOST

Hi

I'm interested in being able to config my DCA1000EVM / AWR1243BOOST setup only via the ethernet (i.e. not use the USB). I see that the hardware of the DCA1000EVM and AWR1243BOOST are prepared for this, with setting some resistores. Do you have, or are you planing to release an FPGA bit-file which is able to do this?

Thanks

/Henric