Hello champion,
I want to use USRR 20m only mode when running the SRR demo. I made below changes to the code:
1) In srrdemo_16xx_mss\common\srr_config_consts.h
comment SUBFRAME_CONF_SRR_USRR, uncomment SUBFRAME_CONF_USRR
/**! @brief The multi-mode Radar mode of operation. */
//#define SUBFRAME_CONF_SRR_USRR /* Two subframes, SRR80 followed by USRR20. */
/**! @brief The USRR only mode of operation. */
#define SUBFRAME_CONF_USRR /* One subframe USRR20. */
/**! @brief The SRR only mode of operation. */
// #define SUBFRAME_CONF_SRR /* One subframe SRR80. */
2) In srrdemo_16xx_dss\common\srr_config_consts.h
same as 1)
After loading the running the new image, I find the DSS assert in line 252 of dss_main.c
gSrrDSSMCB.stats.frameStartEvt++;
/* Check if the previous frame has been completely processed. */
MmwDemo_dssAssert(dataPathObj->chirpCount != 0);
}
Is there any more changes needed to let demo work in USRR-only mode?
Thanks,
Adam
1) In srrdemo_16xx_mss\common\srr_config_consts.h
comment SUBFRAME_CONF_SRR_USRR, uncomment SUBFRAME_CONF_USRR
/**! @brief The multi-mode Radar mode of operation. */
//#define SUBFRAME_CONF_SRR_USRR /* Two subframes, SRR80 followed by USRR20. */
/**! @brief The USRR only mode of operation. */
#define SUBFRAME_CONF_USRR /* One subframe USRR20. */
/**! @brief The SRR only mode of operation. */
// #define SUBFRAME_CONF_SRR /* One subframe SRR80. */