This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/IWR1443BOOST: visualizer won't start automatically

Part Number: IWR1443BOOST


Tool/software: WEBENCH® Design Tools

Hi,

I have adjusted the code to send extra bytes, but now the visualizer won't show my data upon connecting. My script however has no issue receiving and processing the bytes.

The only way i have found to get results from the visualizer is to enter debug mode and start step by step, following by stopping debug mode. the debug mode is found when i inspect the webpage (developer mode).

Even when i stop sending the extra bytes however it won't work.

I have adjusted the code with a hardcoded profile, so it doesn't need to receive a profile before sending bytes. I have tested this with my script that processes the output bytes, and it works. So for some reason the visualizer won't work on startup.

After sending a profile from the visualizer it will receive and process the data.

The lab im using is high accuracy, and i am using the standard high accuracy visualizer, not the fluid one.

Anyway to get this to work immediately?

cheers