Other Parts Discussed in Thread: DCA1000EVM, MMWAVE-STUDIO
Hi,
We are trying to detect static objects inside a cardboard box. Dimensions of cardboard box are 0.5mx0.5x0.5m.
1642 EVM is placed on top of the cardboard box(antenna is facing downwards inside cardboard box).
1. When object is placed in the line of sight of antenna the object is detected
2. When object is slightly moved away from LOS it is not detected by EVM.
3. We are using binary which is provided with sdk 2.0.0.4
We have following queries regarding this
a) We are getting some extra points on scatter plot we think these are reflections from side walls. Is there any solution to get rid of these extra points? For example do we need to have coating of non reflective material in order to detect objects accurately.
b) How can we cover entire box volume inside FOV?
Regards
Vikas