Tool/software: Linux
Using the IWR1443BOOST with ROS. I'm saving the x,y,z coordinates from the pointcloud data to geometry_msgs format and publishing them. There is a difference of 50-60mm in my distance measurements from the ground truth. Reading shown below-
30mm ground truth -> 76mm.
60mm ground truth -> 113mm.
140mm ground truth -> 222mm.
720mm ground truth -> 783mm.
Is this something that happens at lower distances? Or is it a calibration issue?
Also, where does the 0,0,0 lie on the board?
Thank you.