This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDC1000-GASEVM
Hi team,
During the TDC1000-GASEVM test, when set to HV, there are signals on U2-pin5 and U3-pin5 on the green board, but there is no signal after the connected resistors R12 and R22. Why? In this case, RX will also have a pulse output about 3V. Is this normal?
Thanks a lot!
Sherry