This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: How to use Capture Demo to constantly stream LVDS data

Part Number: IWR1443

Hello

I would like to use Capture Demo to constantly stream  LVDS data at 300Mbits/s  DDR  (so CLK frequency 150MHZ) on all 4 lanes

I would like to steam data from ALL RF channels placing each RF channel on a separate lane. 16 bit complex data on each  

I don't know how much I can configure over the CLI to do this?  or how much code needs to be changed?

can anyone help?

Thanks 

 

 

  • Hello,

    For IWR1443, because it has 4 LVDS lanes, each lane will always correspond to one RX.
    As to the setup, can you be more specific on which SDK you are referring to? Why prefer capture demo which only supports limited data in L3 memory?
    Another option is to use mmwave studio which can be used to configure ADC output data rate.

    Thanks and Regards,
    Michelle