This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: CAN bus pinout on the EVM

Part Number: AWR1642BOOST
Other Parts Discussed in Thread: IWR1642, AWR1642

Hello, 

We are making a custom PCB for the IWR1642 IC and we're comparing our schematics with the AWR1642BOOST reference design. 

Now, in the ref design, CAN RX pin of the `1642 is ball D13 (SPIA_MOSI) and CAN TX pin is ball E14 (SPIA_MISO). These pin are also shared with the SPIA functionality using a mux on the board (we ignore that).

However, cross checking with the xWR1642 datasheet, we see that CAN TX is routed to ball C13/C8 and CAN RX is routed to ball E13/B9. Not the same pins as the BOOST reference design.

Can you please elaborate, is this a bug or I misunderstood something ? 

Which BGA balls should I use for CAN ? 

Thanks

Guy