This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642: Boot UART for the IWR1642

Part Number: IWR1642

Hello, 

I'm developing a custom board based on the IWR1642 and have a question regarding booting. 

Which of the uarts (and which pins) does the `1642 use for booting during flash programming, i.e on power up when SOP2 = '1'?

I could not find it in the DS but from the BOOST board I'm guessing these are RX - ball N4 and TX ball N5 as they are connected to external MCU.

Can you please elaborate / confirm ? 

Thanks

Guy