Part Number: OPT8241-CDK-EVM
Hi team.
We are currently testing the OPT8241-CDK-EVM.
If you look at the product specification, the accuracy is indicated as 1mm, but when we test it with VolxelViewer, 5cm ~ 20cm error will occur.
(The farther the distance is, the more error rate is.)
Do We need more parameter settings in VoxelViewer?
Another question will be developed in the scenario below,
Please check if it is possible.
* Products to be developed : Finger touch(writting, drawing) application using 3DToF camera.
[scenario]
1. The computer screen is being printed on the whiteboard with the beam project.
2. 3DTof camera and whiteboard distance(3M) are fixed.
3. The hand of the host and the finger for the finger touch are recognizable.
4. Writable and Drawable when finger touches the whiteboard.
--> When the distance between the finger and the whiteboard is within 5mm, we recognize finger touch.
Please review the possibility of development.
thank you.